Part Number: OPA830 Other Parts Discussed in Thread: OPA381 , TINA-TI , OPA392 Hello community,
I have designed a strain gauge sensor using OPA381 in a bridge configuration in TINA-TI (attached herewith), taking reference from the application circuit of…
Part Number: OPA830 Hello,
I'm designing a sallen-key LPF. The output seems has some oscillation, and the oscillation is always near 0V to DC-bias (above is the input signal and below is the filtered signal).
The oscillation is aournd 50MHz, 11…
Part Number: OPA830 Other Parts Discussed in Thread: TINA-TI , Hi,
Does TI have the IBIS model for this IC that we can provide to customer?
Thank you in advance.
Regards, Maynard
Part Number: OPA830 Hi team,
I was trying to use OPA830 for one of my applications and was willing to understand the transient performance for which I simulated the unity gain configuration for a square pulse as shown below.
I observed that the rising…
Part Number: OPA2830 Other Parts Discussed in Thread: OPA830
Hello, would you please be able to provide details as to the obsolescence of PN OPA2830IDGK? Was the PN replaced with another part? When is the last time buy for this part? What is the longevity…
Part Number: OPA380 Other Parts Discussed in Thread: OPA830 Hello,
I am currently doing an project with transimpedance amplifier for a photodioe, and I would like to test their stability. From some websites, I got an idea that I can verify this through…
Part Number: OPA830 Other Parts Discussed in Thread: LMH6611 , OPA810 , OPA354 , THS4281 Hi team,
Do we have a similar device to the OPA830 with the following parameters:
Single Rail Voltage: ~5-12V
Rail-to-Rail: Input and Output
Output Current: ~100mA
…
Part Number: OPA830 Other Parts Discussed in Thread: OPA837 , LMH6609 , OPA838 I am in a situation where I need to replace an obsolete op amp with a new op amp. I intended to use the OPA830 as this looks to be the best op amp as a replacement however during…
Part Number: OPA830 Hello,
I'm planning to use the OPA830 to drive a clock signal over 50 Ohm coax. The datasheet shows data on VS = +/-5V, 5V and 3V but not for 10V. It does however state that it supports up to a single ended value of 11V.
1. Can …
You are correct, but since these groups are always doing devices for the next rounds of test equipment they always have to do better than anything you can buy. In HD work, source cancellation methods are normally used, one of the very few published references…