Part Number: OPA855 Tool/software: Hi,
i am interested to purchase PN OPA855 in it's die level (not the packaged form)
appreciate if you could quote for me the following quantities:
100
500
1000
in case you do not deal with such request, appreciate…
Part Number: OPA855 Tool/software: Hi,
I am using the OPA855 to create a inverted proportional amplification circuit, but the output signal is behaving strangely. What could be the issue? I am using LTspice software, and the output node is between C3…
Part Number: OPA855 Other Parts Discussed in Thread: THS4302 Tool/software: Hi,
I'm seeking some assistance with an issue I'm encountering in my TIA (Transimpedance Amplifier) circuit based on the OPA855 op-amp. The circuit was previously working well…
Part Number: OPA855 Tool/software: Hi,
I am debugging a TIA circuit, it's a single stage amplifier by OPA855, there are schematic and PCB layout as below:
The circuit outputs a high frequency oscillating waveform when testing in dark environment,…
Part Number: OPA855 Tool/software: Hello TI teams,
Firstly hope all is doing well.
In the case of the implementation of a TIA for SiPM sensor application I tried to simulate a dummy TIA circuit using OPA855 but the output gain is unexpected (very low…
Part Number: OPA855 Tool/software: Hello, everyone.
I am currently going to build a TIA circuit using OPA855, I want to make the TIA bandwidth up to 1.7GHz, and I am designing it based on the values from the TIA calculator. But the bandwidth of the simulation…
Part Number: OPA855 Tool/software: Hello, I made a transimpedance amplifier with opa855.
I use the fast laser pulse(edge time is 1.5ns) and avalanche photodiode(rise time 0.6ns).
So, I have a problem associated with stability.
opa855 is stable with almost…
Part Number: OPA855 Tool/software: Hello, everyone.
I am currently going to build a TIA circuit using OPA855, I want to make the TIA bandwidth up to 1.7GHz, and I am designing it based on the values from the TIA calculator. But the bandwidth of the simulation…
Part Number: OPA855 Tool/software: I use OPA855 with transimpedance amplfier with APD(Avalanceh PhotoDiode).
I want to set proper feedback resistor for wide input signal's dynamic range.
First, I set a feedback resistor to a few hundresd ohm (100…
Part Number: OPA855-Q1 Other Parts Discussed in Thread: OPA855 We are developing Lidar by applying OPA855-Q1. OPA855-Q1 product bandwidth is 8GHz. The PD Bandwidth we are applying is 2GHz. We use the product at 100MHz. Is it possible for the product to operate…