The LM107 regulates the upper LM338 so that the current through the two 0.1 Ω resistors is the same.
This circuit can use any high-voltage opamp whose input common-mode range includes the positive rail. This is not true for the LM741, but the OPA990…
Part Number: OPA170 Other Parts Discussed in Thread: TLV341 , OPA171 , OPA990 Hi, Staff
Customers are currently using OPA170 SOT-5X3 (DRL Package). We are planning to revise the application, but we will not change the board layout.
Customer demands are looking…
Enter 10 V and SC70 into the search function . The TLV9351 and OPA990 are not yet available in the SC70 package. The TLV172/OPA172 do not have rail-to-rail inputs. The LPV511 has a different pinout.
Hello Tim,
Ok. Can you assist us little more on this matter.
We can see that OPA2990SIDGSR is available for ordering/samples on TI, but that this is not going to be in production before March. However OPA990S DBV is going to be in full production in February…
Hello James,
SGM8210 comes in difrerent channel count and packages. So I don't know which one is desired.
I recommend, OPA990, OPA2990, and OPA4990 as replacement devices.
Hello Bhuvaneshwari,
The OPA170AIDBVR is active. You can see that the device is active here .
You can find TI's policy to obsolete a device on our Product Life Cycle web page.
A newer version of the device is the OPA990 and is available in the DBV…
Hi Kevin,
TSX561ILT has RRIO capability along with low input offset voltage, so I recommend OPA990. OPA990 (single channel) will RTM this October, again evaluation can be done with dual channel and replace with a single channel in October.
If the need…