Part Number: OPT101 Hi,
What's the differencebetween OPT101 and temt6000 ?(strength)
Is there a small package of Ambient light sensors like OPT101?
OPT300x is not considered because of the respond time.
Thanks!
Part Number: OPT101 Hello,
i have just downloaded the OPT101 DTL0008A step CAD model. The die/photodiode area is off center with respect to the package (see picture). In the data sheet the active area centre is shown as coincident with the package physical…
Part Number: OPT101 Hello,
the OPT101 datasheet states that "If the light source is focused to a small area of the photodiode, nonlinearity occurs at lower radiant power". Is this due to an intrinsic electric phenomenon or this sentence is explaining…
Part Number: OPT101 Hello, Does the transimpedance amplifier have gain? There is a section in the datasheet electrical characteristics about transimpedance gain, but there doesn't seem to be a spec in dB or V/V.
Thank you.
Part Number: OPT101 Hi, Good day. I hope you are doing fine there. Our customer wants to know if we have a graph that shows the OPT101 Responsivity vs Temperature. For example, if TA = 25 °C and other condition is Ta =30 °C then would the temperature will…
Part Number: OPT101 Dear Sir/Madam,
We are trying to drive the OPT 101 with sine wave in order of kilohertz. As per the datasheet, the -3dB cutoff of OPT 101 is 14 kHz, however, even at the operating frequency of 10 [Hz], we are unable to observe the…
Part Number: OPT101 Dear,
we are designing smoke detector device where we are using OPT101.
Problem : We are facing problem that OPT101 gives output approx. 2.0V after getting green light but this voltage decrees for some time and approx. we find approx…
Part Number: OPT101 i am using opt101 to detect my pulsating light source , i am using single supply configuration and i am getting my signal in this config. but in addition to my positive signals i am also getting a negative peaks. because of this will…