Part Number: OPT3001-Q1 We are using custom board with jetson nano, we need to configure interrupt functionality in opt3301 in latched window style comparison mode, as per data sheet we need to clear a bit every time when interrupt occurs. Can you specify…
Part Number: OPT3001-Q1 Hi team,
Is there any risk to block the I2C if reading the result before a conversion is complete?
Customer set the conversion time to 100ms, and the system will poll the result register(0x0) every 100ms. Any risk?
B&R
Liji…
Part Number: OPT3001-Q1 Hi Expert
because of customer PCB board area limit, customer want to use resistor divide circuit for power to OPT3001-Q1.
so my question is:
Does this device supply requirement high or low? can it accept power supply fluctuate…
Hi Brent,
May you let me know if our OPT3001-Q1 can meet below requirements? End customer is BMW.
1.
Release PPAPs for all locations, if semi-conductor key components with identic product specificaitons are being produced at different Waferprodcution…
Part Number: OPT3001-Q1 From the specification of OPT3001-Q1
Configuration Register Field
bit 11
Field CT
>>The 100-ms conversion time with full-scale ranges below and including 0101b for E[3:0] can reduce the effective result resolution
>>by up…
Part Number: OPT3001-Q1 Hi team,
I would like to confirm with you what is the OPT3001-Q1 internal ADC resolution?
In datasheet, we see the 4-bit Exponent and 12-bit Fractional result, does it mean ADC resolution is 12-bit?
Thanks.
Johnny
Part Number: OPT3001-Q1 Our customer has some question about this item.
When they saw this light sensor EXAMPLE BOARD LAYOUT and EXAMPLE STENCIL DESIGN, there was an instruction to open a Via in the center (Page 42-43), please refer following datasheet…
Part Number: OPT3001-Q1 Hi Team,
question 1
In the project verification stage, my customer will conduct optical related tests on the ALS Sensor, mainly including the response value of the ALS Sensor under different ambient light brightness, and the response…
Part Number: OPT3001-Q1 Other Parts Discussed in Thread: OPT3001 Dears,
I want to achieve the following funciton through OPT3001. When the result register detects that the lux exceeds the value of the high and lower limit registers that I set, INT will…