Part Number: OPT3004 In the datasheet its mentioned 23-bit effective dynamic range however it appears 16-bit resolution in section 8.6.2.1 of datasheet. So what is true resolution of this sensor?
Part Number: OPT3004 We are using the OPT3004 ambient light sensor in a battery-powered Zigbee MCU (EFR32MG24A) product.
The OPT3004 INT pin is connected to the Zigbee MCU and will be used to wake up the MCU from sleep(EM2).
Our goal is to keep the…
Part Number: OPT3004 This is a follow up question on my previous ticket
https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1535659/opt3004-sensor-window-use-of-light-pipe
Can we use right angled light pipe on OPT3004 ?
Do you have…
Part Number: OPT3004 Tool/software: Hi,
I am planning to use the OPT3004 for a day and night detector for my outdoor camera product. See a picture below:
the diameter of the light opening is 5 mm and the distance from the PCB is 12 mm.
Can it…
Part Number: OPT3004 Other Parts Discussed in Thread: OPT3001 Hi,
Our customer is prototyping a product equipped with the OPT3004. They want to slightly correct the illuminance raw data obtained from the OPT3004.
They are using the Linux source code…
Part Number: OPT3004 Other Parts Discussed in Thread: TLA2528 ,
Hi experts!
With the sensor configured as follows:
Range number (RN[3:0]) : Automatic full‑scale mode (1100b)
Conversion time (CT) : 800 ms (1b)
Conversion mode (M[1:0]) …
Part Number: OPT3004 Hello,
My customer is looking for an ambient light sensor solution for indoor and outdoor light measurement, battery operaion.
Please recommend a TI product that meets the following requirements:
- Operating voltage : 1.7-3…
Part Number: OPT3004 Tool/software: Hi team,
My customers are evaluating the OPT3004 and have several problems when using this device. questions are:
1. Under 6500k color temperature, they detected the response is 368.4lux, while this number from…
Part Number: OPT3004 Other Parts Discussed in Thread: OPTISIM Tool/software: Hi,
Is there a tool to calculate the Window mentioned in this document?
Please tell me if there is any other calculation tool for design.
https://www.ti.com/lit/an/sbea002a…
Part Number: OPT3004 Tool/software: Hello folks,
We are working on the universal remote project that uses the OPT3004 ALS.
We are looking for the vendor HAL and integration guide for the OPT3004 ALS with AOSP14.
SoC: Rockchip RK3575
OS: Android14…