Part Number: OPT3101
Hi Team:
In slau791.pdf 3.6.3 Phase offset Ambient coefficient
Phase offset ambient light calibration is required at the determined distance,the ambient light setting parameter in the SDK code is 0;
In this step…
Other Parts Discussed in Thread: OPT3101 Hi Gordon,
From the captured raw data, it can be seen that if opt3101 sends a signal to MCU for data readiness, but MCU's operation to read opt3101 is blocked (multiple opt3101 data readiness signals may pass through…
Part Number: OPT3101 Hi Team:
I have a question:
New hardware needs to be calibrated, following the steps in the SDK; Used OPT3101 Configuration Tool create OPT3101_configuration.cpp file; OPT3101 Configuration Tool Like This:
Open conditional compilation…
Part Number: OPT3101 Hi,
Question 1: Does frequent switching between monostable and continuous modes of OPT3101 affect the repeatability accuracy of distance measurement?
Question 2: In dual frequency continuous mode, after OPT3101 notifies the MCU that…
Part Number: OPT3101 Could you please explain how the amplitude is measured by OPT3101?. What is the formula (describing the relationship between the amplitude measured by OPT3101 and distance) that is used in OPT3101 estimator tool?
Other Parts Discussed in Thread: OPT3101 Gordon:
OPT3101 SDK Performing Internal Cross talk Measurement,I am looking for a text in OPT3101 SDK Users Guide.pdf
The next picture Which parameter of serial port print determines that the internal crosstalk…
Part Number: OPT3101 Hi Team:
There is a question that needs to be answered:
The photodiode used on the OPT3101EVM board is a plug-in, there is no recommended photodiode model of the patch with similar parameters; Use Mini MIDLED package;
Thanks! …
Part Number: OPT3101 Hi Team:
In slau791.pdf,4.2.3 Per unit storing calibrating data in non-volatile memory;OPT3101 does not have non-volatile memory and needs calibration data to be stored in non-volatile memory. One option is to store these settings…
I have an additional question
- Is there a possibility that the "RESEARED" value changes automatically when measuring with OPT3101? Is the “RESEARED” value the same forever? ?
・What is the value of AMPLITUDE that guarantees the accuracy…