Part Number: OPT3101 Hi Team:
There is a question that needs to be answered:
The photodiode used on the OPT3101EVM board is a plug-in, there is no recommended photodiode model of the patch with similar parameters; Use Mini MIDLED package;
Thanks! …
Part Number: OPT3101 Hi Team:
In slau791.pdf,4.2.3 Per unit storing calibrating data in non-volatile memory;OPT3101 does not have non-volatile memory and needs calibration data to be stored in non-volatile memory. One option is to store these settings…
I have an additional question
- Is there a possibility that the "RESEARED" value changes automatically when measuring with OPT3101? Is the “RESEARED” value the same forever? ?
・What is the value of AMPLITUDE that guarantees the accuracy…
Part Number: OPT3101 I can't get dealiasing mode to work. Do you have working source codes for this mode based on the SDK? And for calibration at 8.5Mhz
Part Number: OPT3101 Other Parts Discussed in Thread: TMP102 I have a question about the temperature sensor.
Please tell me the resolution of OPT3101's temperature sensor. Please tell me about TMAIN and TILLUM respectively.
Part Number: OPT3101 While reading the OPT3101 datasheet, I noticed that this chip has average filtering. I want to turn off the average filter. What value should I set for “NUM_AVG_SUB_FRAMES”? NUM_AVG_SUB_FRAMES = 0?1?
Megan,
They did provide me with a fundamental understanding. Also take a look at this document. 5340.OPT3101-Dealiasing.pdf
The basics as explained to me is that the OPT3101 doesnt have register locations for the XTALK and calibration for 2 frequencies…
Part Number: OPT3101
Hi Team:
After completing SDK INLAB_STEP_1, INLAB_STEP_2 and INLAB_STEP_3, the maximum distance measured was only 9m after increasing the crosstalk temperature coefficient. After increasing the phase temperature coefficient, the…
Part Number: OPT3101 Regarding how I use the OPT3101, I perform measurements at a sample rate of 360Hz, and frequently switch between illumination channels Tx0 and Tx1 during sampling. Will switching Tx0 and Tx1 frequently affect the component life of…