Part Number: OPT3101 Hi Team:
There is a question that needs to be answered:
The photodiode used on the OPT3101EVM board is a plug-in, there is no recommended photodiode model of the patch with similar parameters; Use Mini MIDLED package;
Thanks…
Part Number: OPT3101 Tool/software: The OPT3101 detector input is designed to connect to an IR photo diode. We are modifying the detector circuit, replacing the IR photo diode with a visible light solution comprised of a Silicon Photo Multiplier and Transimpedance…
Part Number: OPT3101 I have two questions regarding the OPT3101 register.
opt3101 datasheet ・About his FREQ_COUNT_REG at register address 11h What are the conditions that change the value of this register?
- Read the register from 1h to b9h. The value…
Part Number: OPT3101 Tool/software: Hi Team,
Customer want to achieve Super HDR mode+ de-alias mode, How do we write command to achieve that?
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/1023/_5F00_cgi_2D00_bin_5F00_mmwebwx_2D00_bin_5F00_webwxgetmsgimg_5F005F002600_MsgID_3D00_1826708421553113071_2600_skey_3D004000_crypt_5F00_239a7826_5F00_e6fdd99b6c1f6f416cd554bd00c651ef_2600_mmweb_5F00_appid_3D00_wx_5F00_webfilehelper…
Part Number: OPT3101 Tool/software: Hi,
I am trying to implement the external frequency calibration into my calibration script ( as per OPT3101 Distance Sensor System Calibration (sbau310)).
Custom Hardware.
Opt runs fine without ext freq calib…
Part Number: OPT3101 Hi Team:
I completed the crosstalk temperature coefficient and phase temperature coefficient measurement in the incubator:
After parameter compilation and download, the distance data is not normal, what are the reasons?
Part Number: OPT3101 Hi Team:
The OPT3101 is set to SuperHDR mode. When the distance between the sensor and the target board is tested from far to near, the current channel switching will show a jump from the target distance to far, and it is relatively…
Part Number: OPT3101 Tool/software: on page 83 of SBAS883A –FEBRUARY 2018–REVISED JUNE 2018, in the field descriptions of register 0079h, bit 3, the description is
"Use ILLUM_EN_TX0 for TX1. This mode is required to enable static current-drive mode…
Part Number: OPT3101 Hi Team:
In slau791.pdf,4.2.3 Per unit storing calibrating data in non-volatile memory;OPT3101 does not have non-volatile memory and needs calibration data to be stored in non-volatile memory. One option is to store these settings…