Gordon:
1:Phase offset Ambient coefficient calibration is not to be done in a dark environment?
2:Is this calibration correct? After setting the distance between OPT3101 and the target, use the halogen lamp as the ambient light, adjust the brightness…
Part Number: OPT3101 Hi expert,
Do we have sample code in C language that could be provided for us to better use OPT3101? The reference design and SDK are in C++ code. Thanks!
Joyce
Part Number: OPT3101EVM Other Parts Discussed in Thread: OPT3101 Tool/software: TI C/C++ Compiler Hi,
from on of the query posted at your form i found out sdk of opt3101 for raspberry pi . i want to know if the sdk downloaded from the TI site will work…
Part Number: OPT3101
Hi Team:
After completing SDK INLAB_STEP_1, INLAB_STEP_2 and INLAB_STEP_3, the maximum distance measured was only 9m after increasing the crosstalk temperature coefficient. After increasing the phase temperature coefficient, the…
Part Number: OPT3101 Hi Alex,
1. Where am I suppose to compile the SDK code, do I have to download the MSP430 IDE? I am just confused on how I am suppose to upload the code on to the OPT3101.
2. After I upload the code do I need to use a thermal chamber…
Roberto,
Is all of this about the same issue? Are you still struggling to do the calibration? The calibration is complex but not that difficult.
If it is, I want to dig into your calibration setup. Please describe your setup in detail.
Also look at the…
Gordon:
In my test, MSP-430F5229LP+OPT3101EVM was used for Auto HDR mode test
OPT3101-ConfiguratorTool :
Open SDK conditional compilation INLAB_STEP_0, there is a problem in the serial port print-out data, resulting in an exception in the…
Part Number: OPT3101EVM Other Parts Discussed in Thread: OPT3101 , Hello all,
Here is a little bit information about what I've done so far, to understand where I'm stuck right now.
So I need to develop a sub-system which will give the distance from…
Part Number: OPT3101 I can't get dealiasing mode to work. Do you have working source codes for this mode based on the SDK? And for calibration at 8.5Mhz
Part Number: OPT3101 I'm testing OPT3101 mounted on my hardware: I performed step 2 of SDK Calibration and I found that I changes linearly but Q not.
The circuit uses a LTE-C9506B as IR LED and a TEM1000 as photodiode.
Best Regards
Roberto Cerati