Part Number: OPT4001-Q1 Hi team,
If the light source is 50Hz or 60Hz. Will this type of light source affect the detection of OPT4001-Q1, for example, possibly detecting incorrect low brightness values that differ from what the human eye sees?
The…
Part Number: OPT4001-Q1 Hi team,
Our customer is using a 90 kHz CLK with a rise time greater than 300 ns. According to the datasheet OPT4001-Q1, in Fast Mode, the data rate ranges from 10 kHz to 400 kHz.
Does the signal rise time have to be less than…
Part Number: OPT4001-Q1
Dear TI Representative,
Thank you for your continued support.
When using the OPT4001DNPRQ1 with RANGE REGISTER SETTING = 2 (fixed range) and CONVERSION_TIME REGISTER = 7 (50 ms) to measure the illuminance of an LCD panel…
Part Number: OPT4001-Q1 Other Parts Discussed in Thread: OPT4041
Tool/software:
Hi TI,
Should/could I connect thermal pad of OPT4001-Q1 ambient light sensor in USON-6 package? I mean, can thermal pad be connected to GND or it must remain unconnected…
Part Number: OPT4001-Q1 Other Parts Discussed in Thread: OPT3001-Q1 , Hello Support Team,
This is an inquiry, not an issue. We are currently developing an automotive display driver IC. We are reviewing its specifications to support ambient light sensors…
Part Number: OPT4001-Q1 Other Parts Discussed in Thread: OPT4001 Hello team,
My customer consider to use OPT4001DNPRQ1, but ambient temperature is high.
OEM requirement is below, thus we can think worst case is Ta=110C. Can our device operate such…
Part Number: OPT4001-Q1 Hi team,
ALS is expected to be available in the PicoStar - 0.226 mm max height package. There are some problems in the packaging that need help to confirm PCB cutout recommends irregular shapes. Alternate PCB cut is a circular…
Part Number: OPT4001-Q1 Other Parts Discussed in Thread: OPT4001 Tool/software: Hello team,
My customer want to know OPT4001 output value type.
Could you tell us output value is the maximum or average value of the light irradiated to the photo sensor…
Part Number: OPT4001-Q1 Other Parts Discussed in Thread: OPT4001 Tool/software: Hello,
Using an OPT4001-Q1 sensor on a matrix LED panel (custom design), to estimate ambient light level.
I specifically picked this sensor for its short minimum acquisition…