Part Number: OPT4001-Q1 Hello TI team,
I am working on internal footprint registration process for OPT4001DTSR, and the responsible section is asking me to provide dimension which is not described in drawing of DTS package.
Could you provide me typical…
Part Number: OPT4001-Q1 Other Parts Discussed in Thread: OPT4001 Hello Expert,
Would you answer following question?
Could you explain how to calculate lux from measured result on register using example? Datasheet has explanation but it is using some digital…
Hi Nicole,
when using OPT4001-Q1 EVM, there always exist a fault report as the follow picture,
And the OPT4001EVM is good, do you know why? They need OPT4001-Q1 in automotive.
And could I let customer do the evaluation with OPT4001EVM in this moment…
Part Number: OPT3001-Q1 Other Parts Discussed in Thread: OPT4001-Q1 Hi Team,
I would like to check if our OPT3001-Q1 and OPT4001-Q1 can meet the spec or not. smoke print spec 14%+-4% in 550nm
Regards,
Roy
Other Parts Discussed in Thread: OPT4001-Q1 , OPT3006 , OPT3004 , OPT4001 Hi All,
Iam designing an Android Tablet Hardware.
I need a I2C interfaced compact ALS sensor solution.
Price and driver ability are our main concern.
It seems there are many part …
Part Number: OPT4003-Q1 Other Parts Discussed in Thread: OPT4001 Hello,
I am looking for an optical sensor which can be used behind two-way mirror glass with a thickness of 8.6 mm?
we want to use it to switch lights on and off for an inbuilt cabinet. …
Part Number: OPT4001 Other Parts Discussed in Thread: OPT3001 Hi Team
OPT4001 is the next gen of OPT3001?
what's the difference between this two device, and which sorts of feature was improved of OPT4001 compared with OPT3001