Part Number: P82B715 Other Parts Discussed in Thread: P82B96 , Dear PL application engineer.
one thing need consult associated with P82B715 and P82B96. assume I have two remote I2C DAC(different PCBA board) need interface with my MCU. could I use one…
Part Number: P82B715 Other Parts Discussed in Thread: TCA9800 , , P82B96 , TCA9509 , TMUX154E , TCA9803 , TCA9517 , TCA9617B Tool/software: I want to use P82B715 or P82B96 to extend my I2C bus to about 10m,but the device on remote side work on a voltage…
Part Number: P82B715 Other Parts Discussed in Thread: TCA9617B , TCA9803 , P82B96 The TPS61165DBVR is fully specified for operation down to 4.5 V; however, in our design it is operated at 3.3 V. While operation below 4.5 V is supported, it results in…
Part Number: P82B715 Other Parts Discussed in Thread: P82B96 , , TCA9517A , TCA9617B , TCA9517
Hello Team,
We are currently using the P82B715DR in our product. As part of our ongoing product redesign activities, we reviewed the component lifecycle…
Part Number: P82B715 Tool/software: Hi,
I need the pin capacitance for this IC's data and clock pins for calculating the rise time for my design. Kindly help for the capacitance values.
Thanks
Vinothkumar
Part Number: P82B715 Other Parts Discussed in Thread: TCA9800 , P82B96 , PCA9306 We do not have a long cable or high bus capacitance, but we are considering using two P82B715 devices to solve two other issues in our design:
1. The Vol driven by some…
Part Number: P82B715 Other Parts Discussed in Thread: TCA9617B , LP5018 Tool/software: I'm thinking of using a P82B715 to communicate between an I2C device master and a slave connected by cable.
The I2C device operates on +3.3V.
For example, I could…
Part Number: P82B715 Tool/software: There is a problem with the waveform of I2C CLK
If the 5V power supply of the chip is removed, the falling edge cannot be pulled down.i2c pulls up 1.8V
The 1.8V I2C pull-up was working fine when the normal…
Part Number: P82B715 Tool/software: 1.8V I2C But in the absence of communication, the voltage of I2C is around 2.2V, and during communication, I2C will drop to around 1.8V So the overall waveform presents a stepped shape Under normal circumstances, it…