Part Number: PCA9306 Other Parts Discussed in Thread: LSF0102 Tool/software: A couple of questions relative to the IBIS model
- The IBIS model uses the term "VCC" but the part uses VREF1 and VREF2 - Which does VCC relate to?
- The IBIS model has 5…
Other Parts Discussed in Thread: TCA9416 , PCA9306 Tool/software: Hi team,
Customer is working to design a 1.8V <--> 3.3V I2C level shifter circuit.
They used to use PCA9306, while when I review their circuit, I suggest them goes to TCA9416 based…
Part Number: PCA9306 Other Parts Discussed in Thread: LSF0102 Tool/software: Hi
The main chip works at 8MHz, and we’d like to use PCA9306 for the level shift function. Can PCA9306 works at 8MHz as well?
Thanks
Part Number: PCA9306 Tool/software: Hi Team,
There is a question for PCA9306, on datasheet recommendation, VREF1 supports 1.2 V to VREF2 - 0.6 V, and VREF2 must be between VREF1 + 0.6 V to 5.5 V. If VCC1 = VREF1 = 1.26V. VREF2 = 1.26V + 0.6V = 1.86V…
Part Number: PCA9306
Tool/software:
Hi,
I saw the datasheet that has recommended SCH with 1.8v as Vref1, 3.3v as Vref2..
also found that
VREF2 must be between VREF1 + 0.6 V to 5.5 V in datasheet P5, 6.3 Recommended Operating Conditions
…
Part Number: PCA9306 We have a requirement to address an EEPROM from two different controllers (one at a time). One controller operates at 3.3V. The other controller and EEPROM operate at 2.5V.
Would the attached circuit be the correct way to configure…
Part Number: PCA9306-Q1 Hi team,
My customer would like to evaluate PCA9306-Q1 for I2C signal isolation, refer to the application in the following.
Could you help confirm that when VCC1=VCC2=1.8V, it is possible to connect EN directly to VCC2 via…
Part Number: PCA9306 Other Parts Discussed in Thread: TCA9511A Tool/software: Hi team,
Can PCA9511 and PCA9306 serial connection usage?
Thanks a lot! And looking forward to your reply.
BR,
Matt.
Part Number: PCA9306
Tool/software:
Hello folks, We want to use the PCA9306 as a switched translator and as a switch only.
Will these work? The datasheet isn't very clear on the use of the EN line with an MCU.
What changes if any would you suggest…
Part Number: PCA9306 Tool/software: The datasheet is clear the PCA9306 will work in this configuration:
MASTER----|| PCA9603 ||----SLAVE--SLAVE--SLAVE (i.e. one controller on one side, all other devices on opposite side)
Will the PCA9603 work in…