Part Number: PCA9306 Hello
I am using PCA9306EVM evaluation module to test PCA9306 device to my card.
P ower supply :
VDPU1 = 1.8V.
VDPU2 = 2.6V
Input signals:
SDA1 = 370KHz , level 1.8V
SCL1 = 370KHz , level 1.8V
The output on SDA2…
Part Number: PCA9306 Other Parts Discussed in Thread: LSF0002 Tool/software: Hi team,
My customer want to use 1.8V as their EN LOGIC HIGH level, and I saw the D/S shows the Min as Vref1+0.6(1.8V), Typ 2.1V
Does 1.8V will be too margin to be triggered…
Part Number: PCA9306
Tool/software:
Hi TI team,
This is Allen from Micron product compliance team. I downloaded the TI REACH statement from the website ( Statement on REACH Articles Provisions from Texas Instruments (Rev. AM) ), but it is REACH…
Part Number: PCA9306 Other Parts Discussed in Thread: TCA9406 , LSF0002 Tool/software: Hey team,
Engineer is trying to use PCA9306 as a 1.8V to 3.3V translator for I2C. Issue is, the 3.3V supply will be up before the 1.8V supply.
Ideally, we would…
Part Number: PCA9306 Other Parts Discussed in Thread: TXS0102 , LSF0102 , TCA39416 , TCA9406 , TCA9416 Hi team,
I noticed that the PCA9306 is P2P with TXS0102, and I want to know is there any difference between them, SPEC , function or application?…
Part Number: PCA9306 Other Parts Discussed in Thread: LSF0101 Hello
I am using the PCA9306 to translate from 3.3V I2C to 5V I2C bus. With Vref 1 = 3.3V and Vref2 and EN connects to 5V via 200k res. Is this correct? Is there a capability to simulate…
Part Number: PCA9306 Other Parts Discussed in Thread: TCA4307 , TCA9800 , TCA9509 Hi
The attachment is ltc4307cms8#pbf with PCA9036 to achieve 3.3V to 1.2V, 1 drive 4 function.
There are 2 ltc4307cms8#pbf+PCA9036, each drive 2 FPGas (it is required…
Part Number: PCA9306 Tool/software: Hello.
May it be possible to use this device for lower frequencies than 50 kHz at SCL? In the datasheet are only 100 kHz and 400 kHz mentioned. Figure 9-3 starts at 50 kHz.
Thanks and best regards
Tim