Part Number: EK-TM4C129EXL Tool/software: TI-RTOS Using TIRTOS 2.16.01.04 and CCS v8.
I'm trying to implement an I2C Slave on I2C7, but I'm not getting the expected interrupts, and no ACK is generated for data bytes.
I'm stuck and don't find the…
Part Number: TMDSICE3359 Other Parts Discussed in Thread: AM3359 , TPIC2810 , PCA9536 , SN65HVS882 , TPS65910
Tool/software: Linux
Dear ,
I have booted the ICEv2 board through SD Card but it does not show any ethernet device when I gave ifconfig command and…
Other Parts Discussed in Thread: TMS320C5515 , ADS1298R , PCA9536 , ADS1298 Hi All,
I am trying to connect TMS320C5515 EVM with ADS1298R, and currently I am looking at C5515's Technical Reference:
I can see here that there is only INT1 connected to pin…
Part Number: AM3359 Tool/software: Linux Hello all,
We are bringing up a custom board based on am335x icev2 board.But in our custom board we are using DP83867 PHY chip.We are using gpio3[13] pin as PHY_RESETN.While booting we are getting the following…
Other Parts Discussed in Thread: PCA9536 , TCA6418E , TCA8418E Hi,
I have been looking at I/O expansion for I2C. For an initial prototype I have been using the PCA9536 as I only require 4 I/O pins on my I2C bus. This has all been working fine at 3.3V.
However…
Part Number: AM3359
Tool/software: Linux
Hello all,
I'm working on a custom board based on am335x ice v2.I want to toggle gpio pins at 12MHz.I have learnt that this is not achievable with cortex a8 because of the slow l4 interconnect.We have decided…
Part Number: AM3359
Tool/software: Linux
Hello all,
I'm working on custom board based on am3359 ice v2.The custom board has two ethernet PHYs(dp83867 and max24288).I have added pinmuxing for both.dp83867 is connected to rgmii1 pins and max24288 is connected…
Part Number: AM3359 Tool/software: Linux Hello all,
We are working on a custom board based on am335x icev2.We have connected an additional spi flash at spi1.
spi flash part number:MT25QL256ABA1EW9-0SIT
Connections are :
MCASP0_ACLKX(A13) --> SPI1_SC…
Hi Kemal,
I made the changes you suggested.When i try to probe uboot is crashing and resetting.
U-boot log:
=> sf probe
SF: Detected w25q64cv with page size 256 Bytes, erase size 4 KiB, total 8 MiB
=> sf probe 1:0
data abort
pc :…
am335x-icev2.txt
/*
* Copyright (C) 2016 Texas Instruments Incorporated - http://www.ti.com/
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
…