Part Number: PCI1520 Hi Team,
I have questions regarding PCI1520. I hope you can help.
1. Does this device require a PCI host controller? 2. Can it interface directly to CPU? or WDC65C816S-14? and/or a PIC24 microcontroller? 3. Will it bridge to ISA/XT or…
Part Number: PCI1520 Hello:
We have a project that wants to use TI PCI1520 ghk chip. Please provide the EEPROM data of this chip to us!
Note: pci1520 has two packages: one is QFP and the other is BGA. We need the EEPROM data of BGA package!,Thanks!!!
Part Number: PCI1520 Hello support team
Could you provide PCI1520IZWT thermal impedance information, Theta JA, JC, CA? Customer asks.
Thanks,
Koji Ikeda
Part Number: PCI1520 Hello support team,
My customer need max power consumption , Icc(max) of PIC1520IZWT. Could you support? If there is no spec, assumed value is very helpful.
Thanks,
Koji Ikeda
Part Number: PCI1520 Hi Team,
PCI1520IZWT's Qualification data is not available on TI.com. And CSC could not support this inquiry.
Could you provide the following data?
Material name : PCI1520IZWT
- Qualification summary (included ESD)
- Latch up…
Part Number: PCI1520 The PDV package is mentioned in the PCI1520PDV datasheet but the corresponding page is missing:
8 Mechanical Information
The PCI1520 is packaged in either a 209-ball GHK/ZHK BGA or a 208-pin PDV package. The following show the mechanical…
Part Number: PCI1520 The PDV package is mentioned in the PCI1520PDV datasheet but the corresponding page is missing:
8 Mechanical Information
The PCI1520 is packaged in either a 209-ball GHK/ZHK BGA or a 208-pin PDV package. The following show the mechanical…
Part Number: PCI1520 Other Parts Discussed in Thread: XIO2001 ,
Hi sir,
Does TI have PCMCIA total solution or reference Design?
Need to do a PCMCIA slot, from the CPU's USB & PCIE. which is: USB or PCIe to PCMCIA or USB or PCIE to PCI (or other interface…