Part Number: PCI2050B Hi All:
I use PCI2050B to extend CPCI Backplanes 's slot No.
The appearance as follow :
1,System board insert , i don't insert PCI2050B card,system board can work and power on .I can see winxp desktop on my display .
2,System…
Part Number: PCI2050B Hi all :
I am using PCI2050B ,and i have a question about PCI2050B 's S_CLK.
The datasheet said it should connect with S_CLKOUT9 and the trace length should be the same with other S_CLKOUT to the device .
From PCI2050B to Device…
Part Number: PCI2050B Hi team
Our product have a problem about PCI2050B, the class code we read from the register of PCI2050B is 0600h which is supposed to be 0604h,the vendor ID and device ID is correct. We have already replace a new chip ,but result…
Part Number: PCI2050B Hi TI expert
PCI2050BIGHK is the material that the customer has been using. At present, TI will be discontinued soon.The customer needs us to recommend a new PCI chip. Requirements: frequency 66MHz, 32bit, 3.3V nuclear voltage, reflow…
Part Number: PCI2050B Hello E2E,
Regarding the arbitration algorithm of the PCI bus, the arbitration algorithm is described as "two-tier rotational arbitration" in the data sheet. Regardless of the bus request status of each master, can he eventually…
Part Number: PCI2050B Hello team,
Could you please let me know the theta_JA of PCI2050BPDV?
I found the thermal specs were provided for ZHK package in the previous thread , but I don't find one for QFN.
Regards,
Itoh
Part Number: PCI2050B
Dear Technical Support Team,
Are PCI2050BZHK and PCI2050BZWT the same pin configuration?
These pin pitch and size are same , however number of pins are small.
Best Regards,
ttd
Part Number: PCI2050B Dear TI Team
With EOL for Micro Star BGA products, our customers are considering replacing PCI2050BZHK with PCI2050BZWT. As a result, we have received the following questions, so please answer them.
1. When checking the package, the…
Part Number: PCI2050B Dear TI Team
The following E2E post states that the Micro star BGA products listed below will be released in February 2021, and PCI2050BZHK is also on that list.
E2E: https://e2e.ti.com/support/interface/f/138/t/961193?tisearch=e2e…