Part Number: PCM1681 My customer is looking at PCM1681 for a non-audio application. The data output rate to the DAC channels would be <= 20kHz. Could you please help with the following:
Would it be possible to disable any intermediate processing blocks…
Part Number: PCM1681-Q1 Tool/software: Hi,
I have a customer using the following device, and they had a question about the types of capacitors spec'd in the datasheet. The data sheet calls for two 10uF capacitor caps which should be tantalum or aluminum…
Part Number: PCM1681 Hello,
I have some questions to confirm with you.
1.Two PCM1681 worked with TDM mode, if the I2S data could connect together? Or it is separate connected the TMD data of the front-ended device.
2. Under TDM mode, how to deal…
Part Number: PCM1681-Q1 Tool/software: Hi team,
I would like to check with you if PCM1681-Q1 support TDM8 input? I don't find it in datasheet.
If no, please help recommend the device which have 8ch TDM8 input DAC device.
Thanks!
Ethan Wen
Part Number: PCM1681 Hi Team,
Customer response,
When compiling on different versions of Raspberry Pi systems, the Linux Driver fails. Is there any solution?
Part Number: PCM1865 Other Parts Discussed in Thread: PCM1681 Hello, experts.
The data sheet states that the ratio of externally supplied master clocks (SCKI) to the PCM1865 should be 48%~52%.
In addition, the data sheet states that the ratio of…
Part Number: PCM1861-Q1 Other Parts Discussed in Thread: PCM1681-Q1 , Hi team,
Can PCM1681-Q1 support 6CH TDM? Could you help to provide the related description in datasheet?
BRs,
Haury
Part Number: PCM1681 Other Parts Discussed in Thread: CC2640R2F , CC3200AUDBOOST Hello team,
I am working in a project which it is necessary to use the CC2640R2F I2S peripheral to transmit audio to PCM1681 (or similar) with frequency sample of 48KHz…