Other Parts Discussed in Thread: PCM1753 , PCM1754 Hi all Would you mind if we ask PCM1753 and PCM1754? How much is Group Delay? We could not find it on the datasheet. Kind regards, Hirotaka Matsumoto
Hi Justin,
Thank you for your reply.
We already solved this issue. The root cause is incorrect format(default setting "left-justified").
DS90UB928Q doesn't output "mclk" after locked immediately, But CPU sets format(I2S) for DS90UB928Q.…
Other Parts Discussed in Thread: PCM1753 Hi,
Can we use PCM1753 as the default settings for the registers without setting the registers via the spi interface although we believe that it is possible as below? The pins of ML, MC and MD are floating since…
I came back to my problem. Ii is still actual :(
Is it critical, that sample rate doesn't equal exactly to values from table? I suppose, that only relation between sample rate and SCLK should be satisfied. Correct me if I wrong.
My sample rate is…
Other Parts Discussed in Thread: PCM1753 I am using a PCM1753 to output control voltages to an instrument - one voltage is DC, the other is 10KHz, and I notice that the filtered output covers only about half the full-scale range (I am still in DC test…
Part Number: PCM1742 Other Parts Discussed in Thread: PCM1753 , PCM1741 , PCM1748 it appears that the PCM1742 is a drop in replacement for the PCM 753 , except for the 3.3v volt digital supply. . Is that correct?
Also pin 5 on the PCM1753 is listed a NC…
Other Parts Discussed in Thread: PCM1753 , PCM1807 I want to create a product which uses PCM1807 and PCM1753. They are data converters for audio applications. However, they are complex devices in surface mount package. They require analogue and digital…
Part Number: PCM1755 Other Parts Discussed in Thread: PCM1753 , Is the pcm1755 a drop in replacement for the pcm1753 except for the termperature range?