Part Number: PCM1754-Q1 Other Parts Discussed in Thread: PCM1754 Hi team,
For PCM1754 application, SCK is must need. My customer plan to use an oscillator for SCK input, what is the accuracy requirements? Thanks!
BR
Jiawei
Part Number: PCM1754 Dear Specialists,
My customer is considering PCM1754 and has a question.
I would be grateful if you could advise.
---
I'd like to use FMT fixed at low. Could you please let me know the maximum value of external resistance?
--- …
Part Number: PCM1754 Hi experts:
As the datasheet of PCM1754, its I2S interface is right-justified. And this part support 16bit to 24bit of data. My question is how the device know where is the MSB?
Thank you!
John
Part Number: PCM1754 Hi experts,
If we configured PCM1754 as I2S data format through pulling FMT pin low. The supported data format is shown as figure 23 as below:
The question is, if the audio data is 24-bit and BCK is 48fs, this means the LSB of L…
Part Number: PCM1754-Q1 Other Parts Discussed in Thread: PCM1753-Q1 , PCM1754 , PCM1753 , Hi Expert,
We are getting a problem with this hardware control IC and getting too much distortion over audio because of format mismatch, we have pulled down the FMT…
Part Number: PCM1754 Hello,
Our customer applies Reset when input PCM data Fs is changed. Because in this sequence, sometime PCM1754 is made degradation of SNR issue, and it was solved by Reset.
Here is question, PCM1754 Power On Reset condition is Vcc…
Part Number: PCM1754 Hi Expert,
This is Koki Tsushima.
My customer wants to know about MUTE pin of PCM1754.
Could you answer following two questions?
1. Does 14pin (MUTE) have tolerant functions etc.? Customer think so because absolute maximum rating…
Part Number: PCM1754-Q1 Other Parts Discussed in Thread: PCM1754 , CDCS504-Q1 Hello, Team,
Our customer is adopting PCM1754 in their system. Input data will be I2S and we have a question about SCK and BCK. Fs is 44.1kHz.
Because of the SoC, which outputs…
Part Number: PCM1754
Hi experts,
This is Koki Tsushima.
My customer wants to know detail about this question.
https://e2e.ti.com/support/audio-group/audio/f/audio-forum/1088478/pcm1754-want-to-know-about-mute-pin-of-pcm1754
Could you answer yes or…
Part Number: PCM1754-Q1 Other Parts Discussed in Thread: PCM1754 , PCM1753-Q1 The problem is that if mute pins are turned off, the bottom noise will be there. No matter whether IIS is configured or not, the noise will be slightly reduced by short circuiting…