Part Number: PCM1774 Hi I am using an STM32F7 for audio playing via I2S directly to the PCM1774. It's working perfectly for 20 second and after I get for 4 second an audio with noise. This noise it's came periodically after each 20 second for 4 second…
Part Number: PCM1774 Hi,
I am using the PCM1774 audio DAC for a wearable device and I would like to confirm the schematic for Line output instead headphone.
- Do I need to add a resistor of 10K to the HPOL and HPOR for impedance matching because the RL…
Part Number: PCM1774 Hi,
My customer is trying setting clock frequency as below;
SCLK: 8MHz, FS:31.25kHz, BCLK:1MHz
BCLK/FS=32 in this case.
However, there is no "32" in BIT CLOCK BCK ot table 9/10 on the datasheet.
Does it mean that this setting…
Part Number: PCM1774 Hi,
The default value of NPR and MSR is "0" as below;
On the other hand, All "0" data is nothing on the table9 of the datasheet.
Does it mean that internal PLL is disabled on the default condition?
Best Regards…
Hi Paul,
regarding those question I got already answers:
1 : Yes confirmed is 10k Ω load.
2: When reading the report of the measurement for both stereo and mono output the PCM is about 780mVrms.
3: The signal is a sine wave at 1kHz, no frequency changes…
Part Number: PCM1774 Good morning,
I am currently doing my master thesis in TU Delft and I was thinking of using the PCM1774 as a dual audio DAC to convert the audio data coming from a mini SD card through the microcontroller BeagleBone Black. Do you…
Part Number: PCM1774 Hi :)
My customer wants to use PCM1774 an they do have some questions, maybe you can help.
They would not use AIN1L and AIN1R.
1: What is the recommendation for this two inputs ?
2: is there a recommendation for Ground connections…
Part Number: PCM1774 Other Parts Discussed in Thread: PCM1771 , PCM5102A Hello,
This time, there is Customer who has evaluated PCM1774 as an alternative to Asahi Kasei AK4352. The AK4352 communicates with the microcomputer by using the attached 0: 16bit…
Part Number: PCM1774 Hi!
my customer uses PCM1774 and has the following questions:
------------------------------------------------------------------
PCM1774 is used associated with a Silicon Lab CP2114.
The CP2114 generates 3 clocks to the PCM1774. …