Part Number: PCM1774 This is Joong-hyeok Lee, DMSMS researcher of Leoinnovision. Leoinnovision is the official EOL(End Of-Life)/obsolescence part manager of Korean Military (Army, Navy, Air force) and PLM agency of many defense industries (Hanwha, ADD…
Other Parts Discussed in Thread: PCM1774 Dear,
I am using pcm1774 with cp2114 silicon labs. I want to know if pcm1774 support audio Clock Ratio(MCLK/LRCK) of 250.so that I can use internal oscillator of cp2114
Regards,
Vijayendra
Part Number: PCM1774 Dear Team,
PCM1774 is the 16-Bit Audio DAC, when 32-Bit or 24-Bit I2S Data Format is inputted into the PCM1774, the PCM1774 can receive the audio data normally, without any error, right?
When the audio source data is 24-bit, if Audio…
Part Number: PCM1774 Dear team,
a customer of mine is interested to know if the PCM1774RGPR is UL listed and if it exists, the UL file number.
This is a specific certification from US :
http://database.ul.com/cgi-bin/XYV/template/LISEXT/1FRAME/index.html…
Other Parts Discussed in Thread: PCM1774 Hi
Our customer has a question about PCM1774 DAC gain. He intended to set the gains in 0dB, but measurement gain was 5.1dB smaller than resister settings. The register settings are as follows: address value 0x40 0x…
Other Parts Discussed in Thread: PCM1774 Dear,
I'm trying to generate a 2 KHz beep on the PCM1774 but the sine wave is disturbed (see channel 1). What can cause this mismatched signal?
The audio data format is I2S, no de-emphasis filter and oversampling…
Other Parts Discussed in Thread: PCM1774 On pages 11 and 16, the PCM1774 datasheet mentions the RFM[1:0] bitfield in Register 81, but this register is not documented in the datasheet. Can you provide more information?
Thanks,
Bob Giaraffa
Other Parts Discussed in Thread: PCM1774 Dear,
I want to use the PCM1774 with 1 output as a line out and the 2nd output as a headphone out.
According the datasheet, the impedance of the line out is 10K and headphone is 32 or 16 Ohm. I've configured register…
Other Parts Discussed in Thread: PCM4201 , PCM1774 Hi All, Would you mind if we ask PCM4201 and PCM1774? <Question> These PCM4201 and PCM1774 are used for audio(AC) generally. However, if we use as DC signal(0Hz), are these devices available to use DC signal…