Part Number: PCM1796 Other Parts Discussed in Thread: PCM1804 , TAS5754M HI sir,
Does TI provide Allegro PCB Symbol sharing?
for PCM1796,PCM1804,TAS5754M.
Thanks
Other Parts Discussed in Thread: MSP430F5529 , PCM1796 , PCM9211 Hi all,
i am working on pcm1796 and msp430f5529.
here in pcm1796, pin ZEROL & ZEROR (pin1 and pin2) is connected to microcontroller. when I2S input comes then these pins goes low and when not…
Other Parts Discussed in Thread: PCM1796 HI All,
In data sheet of the pcm1796, zero detection function is available, when i use it, it will not working properly, i try many times to detect and auto mute function when data not come. what can i do for this…
Other Parts Discussed in Thread: PCM1795 , PCM1796 Hi team,
I have compared the user programm fuction control section of both PCM1795 and PCM1796 datasheet, it is almost the same except FMT[2:0] bit is different because 1795 is 32bit and 1796 is 24bit.…
Texas Instruments wide portfolio of Audio features Audio Converters , Audio Amplifiers and other Audio interface devices that are potential crosses for Discontinued, NRND or EOL Cirrus Logic Devices listed by Cirrus Logic here .
TI potential crosses in the…
Other Parts Discussed in Thread: PCM1796 , PCM5102A Hello,
My customer has a question about PCM1796.
[Q]
When PCM1796 does not work, they want to reduce power consumption such as the sleep.
Do you have some ideas?
Can you estimate the power consumption…
Other Parts Discussed in Thread: PCM9211 , PCM1796 , PCM1792 , PCM1794 Hello All, Working over a test setup of DAC using PCM9211 (as digital to I2S converter) and PCM1796 (as I2S to analog converter ). digital to I2S output via PCM9211 is verified and feeded…
Other Parts Discussed in Thread: PCM1796 , PCM1794 Hi,
Can somebody help me? I would like to use the PCM1796 with passive termination. I need 0,4Vpp differential output voltage. I looked for but I didn't find any details about the current segment DAC of…
Other Parts Discussed in Thread: PCM1796 The output stage given in Fig. 36 of the datasheet for the PCM1796 shows a three opamp implementation: a pair of i/v converters on the DAC's differential current output feeding a single opamp diff to single ended…