Part Number: PCM1821 Other Parts Discussed in Thread: PCM1822-Q1 We need to make sure our PCM1821 (or PCM1822-Q1) board is as quiet as possible, but the system we're connecting to is fairly noisy. Thus we want to isolate our analog signals, power, and…
Part Number: PCM1821 Other Parts Discussed in Thread: PCM1822-Q1 , PCM1820 , PCM1820-Q1 If only one channel of the PCM1821 analog input pair is needed, what is the recommended connection for the other pair?
Does this same recommendation apply to PCM1820…
Part Number: PCM1821 Other Parts Discussed in Thread: PCM1804 Hi Sirs, Would you please advise the input offset specification (Vos) of PCM1821 ADC? It is not available in current datasheet in public domain - www.ti.com/.../pcm1821.pdf Thank you and Best…
Part Number: PCM1821 Other Parts Discussed in Thread: LMX2571 , TLV320ADC3120 , , TLV320ADC3100 Hi expert,
My customer is using TLV320ADC3120 with LMX2571 I2S FSK mode.
TLV320ADC3120 can adjust the word length to 16bit. Also LMX2571 input is 16bit…
Part Number: PCM1821 Other Parts Discussed in Thread: PCM1820 I would like to use the PCM1821 with RCA single-ended inputs, but it is not obvious from the datasheet if it will work with IN1M and IN2M connected to capacitors to AGND. Will the 2Vrms input…
Part Number: PCM1821 Hi team,
Typical value of input impedance is 10kHz as the datasheet. Could you share the distribution or similar one? Is the distortion changed by Fs?
Best regards, koyo
Part Number: PCM1821EVM Other Parts Discussed in Thread: PCM1821 Hello,
I'm testing the PCM1821 using PCM1821EVM.
But SDOUT of I2S signal is not working properly.
I have confirmed the signals for BCLK and FSYNC that are working.
Following is…
Part Number: PCM1861-Q1 Other Parts Discussed in Thread: PCM1821-Q1 , PCM1821 Tool/software: I'm using PCM1861-Q1 ADC with H/W conrol mode and I2S format by connection 12.288MHz OSC as below to make a default 48KHz Fs rather than 24.576MHz Crystal. It…
Part Number: PCM1861-Q1 Other Parts Discussed in Thread: PCM1861 , PCM1821-Q1 , PCM1821 , Tool/software: Hi All,
I'm using PCM1861 ADC with H/W conorl mode and I2S format by connection 12.88MHz OSC as below to make a default 48KHz Fs rather than 24…
Part Number: PCM1821EVM Other Parts Discussed in Thread: PCM1821 , PCM4201 , DRV134 Hi
PCM1821 transmits 32-bit two-channel data. The customer's product actually only has a mono signal. When the back-end MCU receives the I2S dual-channel data, it needs…