Part Number: PCM1860-Q1 Other Parts Discussed in Thread: PCM1860 Hi team,
I want to know little more detailed procedure of sample rate change.
I'm confused by "Hold clocks for 3 BCK minimum". If I want to change the fs from 48k to 16k in slave mode, should…
Part Number: PCM1860 Other Parts Discussed in Thread: PCM1840 Good evening.
I am having trouble obtaining exact anti-aliasing requirements of this device. In the datasheet, it is recommended to use a simple, passive filter to attenuate aliased signals…
Part Number: PCM1860-Q1 Other Parts Discussed in Thread: PCM1860 , PCM1861-Q1 , PCM1863-Q1 , PCM1862-Q1 Hello,
My customer was wondering how they should do for the existing system working at Fs=16kHz with system clock of 768fs in slave mode. They'd like…
Part Number: PCM1860 Hi
The datasheet did not make it very clear and I would like to clarify can PCM1860 support 1.8V I2S ? is it correct if i connect IOVDD to 1.8V then the i2S will be 1.8V logic?
Thanks!
Part Number: PCM1860 Hello,
Our customer had evaluated PCM1860EVM and find small pop noise while changing PGA gain from "31.5dB to 32.0dB" or "32.0dB to 31.5dB".
There is no pop noise at the other gain setting and i t is no signal…
Part Number: PCM1860-Q1 Hi Sirs,
I need 8x single end analog audio input, the sampling rate is 16k with 16bit and 1x I2S output. The 8x inputs will work at the same time. so which part of the PCM186x_Q1 can meet my requirement? and what's the sampling…
Part Number: PCM1860 Team,
I am seeing inconsistent pin define inside PCM1860 datasheet. Would you please clarify which one is the correct one?
P.8: P24 is MD3, P23 is MD2
P. 75: P24 is MD2, P23 is MD3
Best regards,
Andy Chu
Hi Dennis,
In PCM1860-1, the source clock frequencies must fit one of 3 pre-defined LRCLK:BCLK ratios. This is determined by the MD0 and MD1 pin to be either 256fs, 384fs, or 512fs.
This is explained in further detail in table 6 of the datasheet.
Regards…
Part Number: PCM1860 Other Parts Discussed in Thread: OPA1632 , PCM4201 Hello sir,
We have plan to use PCM1860 Audio ADC for XLR differential audio line input application.
we have plan to use OPA1632 as a Driver for PCM1860 Audio ADC.
PCM1860 Audio ADC…
Part Number: PCM1860 Other Parts Discussed in Thread: PCM1862 Hi,
I am trying to integrate a PCM1860 to a MediaTek MT7688 SoC that supports I2S for very simple mono audio capturing using only one channel.
Could someone please help me with understanding…