Part Number: PCM1860-Q1 Other Parts Discussed in Thread: PCM1860 Hi expert,
From the Datasheet , we want to kown PCM1860-Q1 Support 4 channel or 2 channel?
Below the picture, we think it support 4channel.
But Below the picture, it seems just support…
Part Number: PCM1860-Q1 Other Parts Discussed in Thread: PCM1861-Q1 , PCM1860 , PCM1862-Q1 , PCM1861 Hello team.
Please tell me about the operation of the INT terminal of PCM1860-Q1.
The datasheet p.8 states the type as [Analog output].
However…
Part Number: PCM1860-Q1 Hello team.
When using the PCM1860-Q1, the gain of the analog signal input section is adjusted.
The data sheet only mentions the typical value of 20kΩ for the input impedance.
Could you please tell me the Max / Min value…
Part Number: PCM1860-Q1 Hello team
The full scale input level in single-ended mode is Max 2.1Vrms, what about the typ / min value?
I want to check the clip of the input signal level and the output digital level.
Ex)
2.1Vrms - 0% / + 15% (3.3V…
Part Number: PCM1860-Q1
Please tell me about the start and end sequences.
I am thinking of starting and terminating by Power-On Reset.
According to the data sheet P.81, after the voltage value of the internal LDO is 1.5V and the [LDO_GOOD] flag…
Part Number: PCM1860-Q1 hi, when analog supply is 3.3V and IO supply is 1.8V, which should come earlier? Or there is no such limitation? also in this supply use case, are there any concern if MCLK input to XI and use 44.1kHz sampling? (just double check…
Part Number: PCM1860-Q1 Hello,
I have some question about [7.11 Timing Requirements: Audio Data Interface for Slave Mode] in datasheet P.18.
** Our using Condition**
at TA = 25°C, AVDD = 3.3 V, DVDD = 3.3 V, IOVDD = 3.3 V, slave mode, fs = 16…
Part Number: PCM1860-Q1 Table 1 in the datasheet describes the HW pin settings that produce different channel routing.
First, we’re receiving differential signals. The table seems to imply that reading Ch 3 and Ch 4 always introduces +12dB Gain re:…
Part Number: PCM1860-Q1 Hello team.
Please tell me about GAIN switching during IC operation of PCM1860-Q1.
In order to switch the gain of CH4, we plan to switch the logic of MD6 pin, MD5 pin, and MD2 pin during IC operation.
Does this use cause…
Part Number: PCM1860-Q1 Other Parts Discussed in Thread: PCM1860 , PCM1865 , PCM1863 , PCM1862 , PCM1864 Hi TI,
Does PCM1860 support analog input mix? I have checked the block diagram as below. It seems there are mix and mux function for analog input…