Part Number: PCM1862 Other Parts Discussed in Thread: PCM1864 , Hello,
I changed from the PCM1864 to the PCM1862. Analog input pins 1L and 1R are used and muxed to the first Audio ADC, but both Digital outputs DOU and DOUT2 are used. When using the…
Part Number: PCM1862 Other Parts Discussed in Thread: TAS5825M , PCM1808 , TLV320ADC3140 Hi Sir,
My customer looking for ADC after TAS5825M(with LC filter), would you pls help recommends which ADC is suitable under condition?
Condition of TAS5825M…
Part Number: PCM1862-Q1 Other Parts Discussed in Thread: PCM1862 , , PCM1860-Q1 , PCM1840 , PCM3168A Hi
Since customer needs TDM, and two or four simple channels audio ADC, no gain control is needed. Does PCM1862-Q1 work without I2C Configuration? Or…
Part Number: PCM1862 Tool/software: Code Composer Studio Is there a PCM1862 I2C software configuration reference program available?If not, is there any documentation available?
Part Number: PCM1862 Hi Team,
Is I2C interface logic voltage level change to 1.8V with 1.8V IOVDD supply for PCM1862?
Background : I use 3.3V IOVDD in other board in the past which I2C communication works well. And when I make a new board with low…
Part Number: PCM1862-Q1 Other Parts Discussed in Thread: PCM1862 1. If PCM1862 uses TDM cascade, does it support 12-channel microphone input?
2.If PCM1862 uses TDM cascade, does it support 12-channel microphone input?
Part Number: PCM1862 Other Parts Discussed in Thread: PCM1864 I have a customer that wants to change from PCM1862 to PCM1864. I know they share a DS and it seems that they will get the same performance without the need to change drivers or use a different…
Part Number: PCM1862 Hi,Ti
When I was using PCM1862, the SCKI input was always 12.288MHz, and the relevant registers were set as follows:
(0x2a): 0x1 (0x2b): 0x8 (0x2c): 0x0 (0x2d): 0x0 (0x29): 0x1
Under this configuration, the sampling clock should…
Part Number: PCM1862 Hello, expert,
I received question about Clock Halt and Error Detect for PCM1862.
When CLK was changed without CLK halt as follows, from 44.1kHz x to 48kHz, will it be regarded as CLK error?
SCLK 22.579MHz ⇒ 24.576MHz…
Part Number: PCM1862 Hello Team,
My custom wants to detect the loss of input audio signal in the active mode of pcm1862. At present, the function of playing music in pcm1862 can work normally after being configured, but the interruption signal of pin19…