Part Number: PCM1863 Other Parts Discussed in Thread: TLV320ADC5140 Hello,
We plan to use PCM1863 in Slave mode with BCK reference input PLL mode to generate SCK. And output SCK from GPIO1 to external PCM-DAC SCK input.
In this case we will set following…
Part Number: PCM1863 Hello TI Engineers,
Regarding the PCM1863, what is the state of the mic bias at power up? On or off?
I have looked through the datasheet and can not find this information.
Kind regards,
Jeffrey Bruton
Part Number: PCM1863 If I can use 8 input channels in parallel with one channel analog single inputs. That means connecting the eight channels in parallel
Part Number: PCM1863 Hi team,
Based on DS, section 12.7, shows 2 cases 3.3V of all supplies or separate, do you have any sequence requrement when start-up/shut-down?
Do you have any limitation for raising /falling time of AVDD/DVDD/IOVDD at those time…
Part Number: PCM1863 Other Parts Discussed in Thread: PCM1864
Hi Team,
My customer occurs a abnormal phenomenon when using PCM1863. Customer uses VINL2 and VINR2 as input. The PCM1863 works in master mode and MCLK is 12.288MHz, BCLK is 6.144MHz, LRCLK…
Hi Carson,
The additional file is the 2V test data, and the test results of different inputs of 200mV are attached. What other test items need? In addition, We have a desoldering PCM1863 exchange between the two PCBs,Low CMRR issue is follows IC, how to ensure…
Part Number: PCM1863 Hi TI Team, I have a question,PCM1863 0DB signal equal to how much analog differential input?PCM1863 0DB signal equal to how much analog single-ended input?
Part Number: PCM1863 Hi team,
I wants to know the PCM1863 VINL1/VIN1P PIN input range when it is configured as single-ended mode. In datasheet 7.1 Absolute Maximum Ratings, VINxx to AGND voltage should be in the range of -1.7V ~ 5V.
But in EVM test, we…