Part Number: PCM1864-Q1 Other Parts Discussed in Thread: PCM1864 Tool/software: Hello:
At present, the mic interface channel has been adjusted in sample B. Sample B is only connected to two channels of MIC. The DOUT of PCM1864 in sample B has no output…
Part Number: PCM1864 Other Parts Discussed in Thread: TIDA-01454 Hello Experts,
Regarding the TIDA-01454, I just have a few points of confusion: 1. Is it strictly necessary to share the I2S master clock between the two PCM1864s? I don't see a connection…
Part Number: PCM1864-Q1 Other Parts Discussed in Thread: PCM1864 Tool/software: Hello:
The customer used TI's Audio ADCs PCM1864Q and needs to provide the relevant driver and register sequence for qnx initialization. The customer stated that the reference…
Part Number: PCM1864-Q1 Other Parts Discussed in Thread: PCM1864
Run the following command multiple times to read the register values of the PCM1864Q1 ADC chip. i2cget -y -f 33 0x4a 0x72 i2cget -y -f 33 0x4a 0x72 i2cget -y -f 33 0x4a 0x72
[Observed…
Part Number: PCM1864-Q1 Tool/software: Hi team,
When the customer's IOVDD is powered by 1.8V, is the high-level amplitude of the TDM signal 1.8V or 3.3V?
Part Number: PCM1864 Tool/software: Hi,
Could you tell me how how to calculate DC voltage from PCM1864's Secondary ADC value.
I want to get DC voltage from VINL1 input pin.
AUXADC_DATA_CTRL register(Register 88) was written value 0xF0.
Secondary…
Part Number: PCM1864 Hello TI experts, While working on a maintenance firmware release for one of our more popular products, I decided to look into a bug that is seen only on a very small percentage of the manufactured units. The failing units appear…
Part Number: PCM1864 Hi,
I would like to know the best possible way to interface PCM1864CMB with 280049C launch pad. I would like to complete the basic evaluation of the Circular Microphone Board with the DSP device.
Thanks for your support.
Part Number: PCM1864
Hi team,
can you help to review the PCM1864 schematic?
customer would like remove osc crystal, and use BCLK as reference clock, please help check if it can work?
thank you
1321.PCM1864.pdf
Part Number: PCM1864
Dear team,
I want to know the RMS noise level for PCM1864? I try to use the SNR parameter to calculate as screenshot below.
But I find from the figure below is about -140dB.
Could you guide me to find right way to get…