Part Number: PCM1864EVM Other Parts Discussed in Thread: PUREPATHCONSOLE Hi,
Many Thanks in advance. I have installed PurePath Console so that I can check my PCM1864EVM ADC board, but the only available app is the i2c generic master. I have no idea about…
Part Number: PCM1864EVM Other Parts Discussed in Thread: PCM1864 I am using the PCM1864 as the master using J8 and J10 jumpers as specified in the manual.
I set up a generic ALSA i2s device tree using 'simple-audio-card', I can see the device using arecord…
Hi Daveon-san,
Thank you for your continuous support.
I understand that "the inital clock divider shown in "Master Mode Only" box should not exceed the 24.58Mhz crystal frequency". However, what does it mean that "Best practice is to restart the EVM when…
Hi Juan,
A few things for your Arduino code-
1. When calling begin transmission from the wire library , be sure to input the device address into the function.
2. Since the sound sensor board produces a changing voltage, you'll need the Arduino’s analog…
Part Number: PCM1864EVM Other Parts Discussed in Thread: PCM1864 , PUREPATHCONSOLE I loaded PurePath Console2, version 2.1_r35934 a couple of months ago to work with the PCM1864EVM. It launched successfully and I could control the EVM. I used it for several…
Other Parts Discussed in Thread: PCM1864 , PCM1864EVM , PCM1865 Hello,
is this possible to change mode using Linux?
The main target is to record all four channels with the use of a BeagleBone Black and save recorded file on a SD card. I know that USB to I2S…
Part Number: PCM1864EVM Other Parts Discussed in Thread: PCM5102A
Hi Team,
Customer is having trouble in implementing their application in PCM1864EVM. Below is the details.
"
We are using PCM1864EVM with combination of Beaglebone Black to access…
Part Number: PCM1864EVM Other Parts Discussed in Thread: PCM1864
Tool/software: Code Composer Studio
Dear,
our client use PCM1864CMBEVM + EVMK2G , But we find the BF tool only support 8KHz and 16KHz, it`s could possible can support sampling rate to 40KHz…