Other Parts Discussed in Thread: PCM2704 Hi All,
I want to play FLAC(Free Lossless Audio Codec) library using the PCM2704 or PCM2704EVM.
Is it possible?
Regards,
Seishin
Other Parts Discussed in Thread: PCM2704 Can we get a hold of a USB Audio Driver for Windows Embedded Standard 7. We are using our old ATI with the TI PCM2704DB USB Audio device in it … and we need the driver.
Other Parts Discussed in Thread: PCM2704 Hello, i just build DAC with PCM2704. Everything work good until I connect EEPROM. My ROM is BR24L01A-W type with loaded data examle from PCM2704 datasheet. But nothing is doing. Address of ROM is set to 0x50. On…
Other Parts Discussed in Thread: PCM2704 Hi,
I am using a PCM2704 with both XP and Win 7, same issue with both. When I disable the PCM2704's USB port, there is a distinct "pop" out the speakers. Has anyone else run into this issue, and if…
Other Parts Discussed in Thread: PCM2704C I'm designing an external sound card based on the PCM2704C and I would like to know if any Android device with 4.X SW (regardless of tablet or smartphone) will "see" the sound card and stream audio to it.…
Hi Cindy
for Analog in to SPDIF PCM9211 is the best solution. we don't have a single analog to SPDIF solution.
for USB to SPDIF converter PCM2704/05 has this ability.
Regards,
Arthur
Part Number: PCM2912A Other Parts Discussed in Thread: PCM2704 , PCM5102A , PCM5100A , PCM5122 , TPA6120A2 , TLV320AIC3253 , TLV320DAC3203 , PCM1771 , PCM1770 , PCM1774
Hello,
I'm looking for a DAC with headphones output and I2S interface (or any other interface…
Part Number: PCM2704C Other Parts Discussed in Thread: PCM2704 , TPA3138D2 , , PCM2900 Hey all,
A customer is having issues with the PCM2704 EVM:
"We are currently using the PCM2704C EVM with the TPA3138D2 EVM for testing, and the volume control buttons…
Other Parts Discussed in Thread: PCM2704 , TPA6120A2 , TPA6132A2 Hei.
I plan to use the TPA6120 behind a PCM2704 for a more Powerfull Output Stage.
Now the Question is, can i use the VCOM Output of the PCM2704 (the Virtual 0 of the DAC) for the 0V on a…
Other Parts Discussed in Thread: PCM2704 In the PCM2704 data sheet, distortion figures at different load resistances (impedances?) are given - distortion is higher at lower impedance.
In the supplied reference designs, something resembling a 'Zobel network…