Part Number: PCM2706 We're connecting the PCM2706 (USB audio CODEC) to a TPA2011 (analog class-D amplifier). It looks like we should be able to connect one of line outs from the PCM2706 to in+ on the TPA2011, and VCOM from the PCM2706 to in- on the TPA2011…
Part Number: PCM2706 Other Parts Discussed in Thread: TAS5713 , , TAS5754M Hi Steve, I was trying to make an I2S demonstrator using a PCM2706 evaluation module from AliExpress and a TAS5713 soldered to a breakout-board.
The I2S signal generated by the…
Part Number: PCM2706 Other Parts Discussed in Thread: PCM5102A , Develoment envirment: windows7, PCM2706C i2s output, pcm5102A DAC
when i stop to play the music, the pcm2706c will output about 10s I2S signal, and this will cause weak noise in next DAC, …
Part Number: PCM2706 Hi all,
In sleu116.pdf in the schematic "Figure 2" there is a AT24C64N Flash connected to the PCM2706/7.
This type of flash needs 2x8 bit address to read/write.
But as reading external USB-descriptors did not work out in…
Part Number: PCM2706 I would like to slave a PCM2706's I2S interface to my audio processor's MCLK.
Is there a configuration option to make the I2S interface operate in slave mode ?
Thanks in advance,
Charlie
Hi again,
Do you have a schematic that you would recommend following? I feel like I have tried every combination, and can't get it to work upon reset / power cycle. I am using the TUSB2046B hub with the PCM2706. The power management is using the TPS2044…
Other Parts Discussed in Thread: PCM2706 Dear Sir
We uses PCM2706 Audio DAC for USB MP3 player.
So far we encountered a problem need your help to clarify. below is our schematic file
http://www.seawalk.com.tw/0000/2.html
When we turn on the system power…
Other Parts Discussed in Thread: TUSB2046B , PCM2706 , PCM2900C Hi all,
I am starting a project with using the PCM2900C as well as the PCM2706 and the TUSB2046B. And the question I have, is there an advantage to either powering via the USB Bus, or to self…