Other Parts Discussed in Thread: PCM2900B , PCM2903 , PCM2900 Per the datasheet...it appears that we can run the PCM2900B off our board 3.3V supply...and not use VBus for this. Are there any downsides to connecting it..ie...it wont show enumeration until…
Other Parts Discussed in Thread: PCM2900B Hi,
I am working on a project to capture some low frequency signals and I am using the PCM2900B. I built the circuit as suggested in the datasheet for the "simple application", however, when I plug it into the…
Other Parts Discussed in Thread: PCM2900B , DRV632 , TPA6138A2 The data sheet specs out this part is supposed to have a SNR on the DAC of 96dB, but we are measuring closer to 70 with our Audio Precision. There is no amp stage, this is right out of the PCM2900B…
Other Parts Discussed in Thread: TUSB2077A , PCM2900B , MSP430F5510 We have a design with TUSB2077A hub, down stream with the followings:
- PCM2900B codec
- MSP430F5510
- PIDUSBD12 from Philips/NXP/ST Ericson
other 4 ports are open.
The codec PCM2900B…
Part Number: PCM2900C Other Parts Discussed in Thread: PCM2900B , Hi,
My customer is seeing PCM2900C detected as Line (USB AUDIO CODEC), PCM2900b detected as Microphone (USB AUDIO CODEC). PCM2900C value/level is also half that of PCM2900B. I will loop in…
Other Parts Discussed in Thread: PCM2900B , PCM2900C I have used the PCM2900B in a design but it only works with Windows XP
I have tried the PCM2900C and it works with Windows 7.
Is there a difference in the signal levels (for a given digital value) between…
Other Parts Discussed in Thread: PCM2900B , PCM2900C , PCM2900 , TUSB2046B I replaced a PCM2900B with a PCM2900C and now Windows 7 does not recognize the device.
It cannot find the driver.
I have uninstalled the device and restarted the computer.
Still…
Other Parts Discussed in Thread: PCM2900B , PCM2902B , PCM2902C Hello everyone,
I was thinking about connecting a simple usb mp3/wav player in my LM4702C based power amplifier, someone knows about some IC or ICs that I can use to do this task, I want something…
Hi Alex,
The PCM2900C is compatible with Windows 7 and compliant with USB 2.0. The application note below details all the changes between the PCM2900B and PCM2900C. The PCM2904 is similar to PCM2900B so, some of the big differences should be similar…