Part Number: PCM2902 Other Parts Discussed in Thread: , PCM2900 Dears,
We use PCM2902 for codec, have two input channel, USB for digital and analog path; there have noise in output when chose analog input path, do you have advise for this issue, thanks…
Part Number: PCM2902 Other Parts Discussed in Thread: PCM2912 , I built an audio interface with a PCM 2902(E), about 7 years ago. Originally it worked with no problems. But with more recent PCs/versions of windows (eg more recent versions of WIndows 10…
Part Number: PCM2902 I have built an audio interface with PCM2902E. This worked perfectly with Android versions about 5 to 9 via an OTG cable, and with some earlier versions of Android 10. I thought perhaps the PCM2902 was too old to deal with newer OSs…
Part Number: PCM2902C Other Parts Discussed in Thread: PCM2902 , Hello.
We are successfully using PCM2902 for years in our measurement environment and would now like to redesign a circuit with PCM2902C.
One of our user complaints is about the driver or…
Part Number: PCM2902 I'm a hardware developer. I'm having trouble developing a capture device with pcm2902. The client when installing the windows drive by default configures as MIC input as Mono. Is there any way to modify the driver so that the windows…
Part Number: PCM2902 Other Parts Discussed in Thread: PCM2903 Hi,
My company has the PCM2902 in a number of designs, and I've been tasked to come up with a way to automate the audio testing, both input and output, of this particular component. I'm…
Other Parts Discussed in Thread: TL082 , PCM2902C HELLO, I have build audio interface for guitar input using PCM2902C. for pre amplifier i'm using TL082. When i'm choice sampel rate 48KHz the device capture much noise and distortion but when choice under…
Part Number: PCM2902 Hello, I have an oscilloscope project in the sound input of the PC together with LabView, in which I want to make a circuit for it to work with PCM2902. But the circuit that I set up following the base of the datasheet captures a…
Other Parts Discussed in Thread: PCM2902C Hello,
I am aware that the internal DAC is 48Khz, but if I take digital out and bypass the internal DAC am I also limited to this sample rate?
Many thanks,
Stephen
Part Number: PCM2902C Other Parts Discussed in Thread: TAS2780 , , PCM2902 , DIR9001 Goal: USB Audio & Audio amp.
Planning to use a PCM2902C SPDIF output into a TAS2780 (25W Class-D audio amp)
but the TAS2780 takes in a TDM signal while the PCM2902 outputs…