Part Number: PCM2902C Other Parts Discussed in Thread: PCM2902 Good morning.
We are looking for external USB sound cards with the PCM2902 chip or similar from the same PCM290x family.
Is it possible for someone to provide us with a reference?
Thanks in…
One more question about PCM2902C
We put the analog inputs on the PCM2902 as stereo to R and L. A signal that is a mixture of the two signals is being output as an output. Now, a code is applied to separate the two signals by detecting the channel of the…
Part Number: TPA3138D2 Other Parts Discussed in Thread: PCM2902 , PCM2902C , Hello,
We are working on the design of usb speaker out. We are planning to use the PCM2902 and its output we are planning
to use the TPA3138 for audio amplifier for 5W output.
…
Other Parts Discussed in Thread: PCM2902 I am a bit confused about how the PCM2902 ADC inputs work., but hope that you can put me on the right path please. I am trying to use the PCM2902 as a ADC to SPDIF and/or USB input converter, My intention is to…
Other Parts Discussed in Thread: PCM2902 Hi,
Is it possible at all to suspend an individual PCM2902 in a working "live" system?
Microsoft is talking about "Selective Suspend" but we have not been able to find anything to test this, even…
Other Parts Discussed in Thread: PCM2902 , PCM2902B , DIR9001 , DIX4192 Hi all !
I have a question about the PCM2902 chip; it's possible to use the same as analog audio to SPDIF converter without connect the same to a USB port ??? and powered it with an external…
Part Number: PCM2906C Other Parts Discussed in Thread: PCM2902 , I would like to use the PCM2906C to accept two input channels and output 4 signals. My customer is reporting that the Behringer UCA202, based on the PCM2902, is able to offer a headphone jack…
Other Parts Discussed in Thread: PCM2902 I've been looking at the PCM2902 ( http://focus.ti.com/lit/ds/symlink/pcm2902.pdf ) ADC and I'm wondering what the input impedence of the chip is in the off state? I'm concerned that if powered down, the chip may…
Part Number: PCM2912A Other Parts Discussed in Thread: DIR9001 , PCM2902 hi,
is there any device which can support audio signal with USB interface and transfer to I2S interface, such as CP2615;
CP2615: www.silabs.com/.../device.cp2615;
Hi Collin,
If we connect the Hisilicon palyer SPDIF to the Yamaha Power Amplifier,it is OK.
But connect to the PCM2902,it does not work. Hi3798M V200 Data Sheet 01-General Information.pdf