Hi Conor,
Internal records aren't 100% conclusive on this because again the device is quite old, but it appears like there wasn't a revision released to address this bug.
Part Number: PCM2904 Hi,
I would like to inquire about PCM2904, but since it contains confidential information, is it possible to contact an expert privately?
Thanks,
Conor
Part Number: PCM2904 Other Parts Discussed in Thread: PCM2901 Hi,
The standard way to use the PCM2904 is to use it with bus power.
We are considering using cell power. Is it okay to use the PCM2904 on its own with a dedicated power supply IC? It is assumed…
Part Number: PCM2904 Hi All
As part of the project, I need to decide whether I will separate ground planes under PCM2904 or not.
The Power 5V planes were separated accordingly.
Please see the image: separated groundes with a simple ferrite bead that can…
Part Number: PCM2904 Other Parts Discussed in Thread: PCM2906B , , PCM2906C Hello,
My customer has been investigating PCM2904, but as you know it has inter-channel phase difference issue, so they asked me if there is an alternative IC fixing the issue. …
Part Number: PCM2904
Hi,
Good Day.
Customer is having a built prototype USB stereo input interface with PCM2904.
Works OK with Windows 7 and 10, but tried on Microsoft GO with Windows 11 and it says does not recognize it?
Any advice please (Selected…
Part Number: PCM2904 I would like to use PCM2904 as two channels acquisition device.
I have built the circuit according to the schematics shown in figure 38 of the datasheet.
I manage to acquire correctly the input VinL (pin 12). However, I don't see…
Part Number: PCM2904 Other Parts Discussed in Thread: PCM2900 , PCM2906C We have noticed that there is some severe ciipping on the output of the PCM2904 chip. We are inputting a standard Wave file, and the output appears to be 2.9V peak to peak which implies…
Part Number: PCM2904 Other Parts Discussed in Thread: PCM2912 , TL072 Hello,
I've successfully built the PCM2904 circuit from the datasheet, I can hear audio coming out and I can record audio if I loop the PC output. My question is, can I build an amplifier…