Part Number: PCM2906C Hi team,
My customer wants to find a device that can convert USB digital audio signal to analog audio signal. I find PCM2906C might be proper here. But in customer's system, the USB host side is a Linux OS. So can you help check…
Part Number: PCM2906C We are connecting multiple (up to 4) devices that are based on PCM2906C Audio Codec to one linux machine. The devices are properly detected as audio cards and sensor-data can be recorded from them via an ALSA API.
Now we need a…
Part Number: PCM2906C Hello,
I'm researching for an audio codec with SPDIF or PDM input and output.
This is for a project involving audio recording/playback and the requirement for SPDIF/PDM is because all I2S interfaces of the DSP are already in…
Part Number: PCM2906C Other Parts Discussed in Thread: TPA3110D2 , HI,
We have a problem with our audio design, based on PCM2906C and TPA3110D2. This is a part of bigger product, run with WIN10 OS.
PCM2906C is our USB audio card. We have noticed strange…
Part Number: PCM2906C Other Parts Discussed in Thread: PCM2902C , Dear Team,
May you help to check some suitable solution for our customer? We appreciated your great support.
Please help to consult them about the requirement below.
USB2.0 full…
Part Number: PCM2906C Dear TI support forum
i am looking a application , using 2 number of PCM2906 , feed 4 MIC inputs and wants to connect a USB o/p to a PC , for recording 4MIC
My question is ,,how 2 combine, 2USB o/p from 2 PCM2906 ..into 1 …
Part Number: PCM2906C Hi team, Will the suspend status continue even if there is no power supply to VCCCI(10pin)? In the other words, if there is only VBUS (3pin), will this mode continue? It is designed with reference to Fig.36, and my customer are considering…
Part Number: PCM2906C Very simple question:
Can I use the PCM2906C without the LPF_AMP on the IN and OUT and still get the LINE IN and LINE OUT audio?
(We won't connect the circuit to any speaker system, we need only to record proper audio from a…
Part Number: PCM2906C Dear folks,
I need aSPDIF interface and selected the 2906C.
I used the schematic that is in the datasheet.
If I understand it correctly, one simply plugs the
usb into the connector and some sort of a driver
will be installed…
Part Number: PCM2906C Hi,
I'm driving SPDIF OUT of the ADAU1452 chip (specifically the EVAL-ADAU1452REVBZ evaluation board). I have confirmed operation of the PCM2906 EVM when I drive an analog input into it and can see the resulting output in Audacity…