Part Number: PCM2906C Should all ground pins on the codec be tied to the same net? I have an audio ground that runs off my amplifer and I was thinking to tie the analog grounds of the codec here, but couldn't tell from the block diagrams how the digital…
Part Number: PCM2906C Hello,
My customer wants to use PCM2906C but I found a thread saying it's not UAC 2.0 compatible. Do we have any similar devices that are compatible with UAC 2.0?
Thanks,
Michael
Part Number: PCM2906C Dear Sir/Madam,
I wondered if DC coupling of the ADC inputs is possible on the PCM2906C when the signal is level shifted by Vcom using external circuitry?
The rationale behind it being that the coupling capacitors could be left out…
Part Number: PCM2906C Hello,
I am designing a circuit using the PCM2906C and in the eval circuit I see that the suspend signal from the codec is connected to the enable circuit of the regulator and this same circuit powers the input amplifiers. If the…
Part Number: PCM2906C Other Parts Discussed in Thread: PCM2902 , I would like to use the PCM2906C to accept two input channels and output 4 signals. My customer is reporting that the Behringer UCA202, based on the PCM2902, is able to offer a headphone jack…
Part Number: PCM2906C Hi, the PCM2906C may rec and play simultaneously in analog in and outs?
The question is for use in an audio editing program.
Thanks.
Ariel Heredia.
Part Number: PCM2906C Hi, I was trying to build a really basic circuit based on the PCM2906C to record audio in my computer, the problem is that when I try to plug it into the computer the third pin of the ic (VBUS pin) starts to smoke. I just wanted…
Part Number: PCM2906C Hi, we have design the audio codec module based on PCM2906C. Using the reference gerber and evaluate board technical documents we design our own PCB.
Our query is ..to make the new pcb functional..do we need any specific software…
Part Number: PCM2906C I have a design that requires 2 x PCM2906C for 4 inputs and 8 output channels. I'm looking to use an external source for VCCI on my PCM2906C design to put it in high performance mode. I have a AP7361C-FGE-7 regulator set to output…
Part Number: PCM2906C Hello,
Regarding to 4ch analog output on PCM2906C, my customer is asking a question.
They will use two PCM2906C for 4ch analog output. (USB data is sent via HUB from PC.)
(Question)
Can PCM2906C support mult-channel USB audio? …