Part Number: PCM2912A Other Parts Discussed in Thread: PCM2912 Hi
Could you help check the PCM2912 schematic as below and any need to adjust?
Thank you
Part Number: PCM2912
Hi, I'm a designer who works at Leonardo S.p.a.
We are using in our product, your component, the Codec PN: PCM2912 with the USB port not direcly connected to the USB port of PC (OS: Windows 7 professional) but using USB / LAN…
Part Number: PCM2912A HI!
When the PCM2912A is connected to a PC, the playback and recording functions are activated in the control panel menu. But my client wants to disable playback and make it invisible in the menu. Can I get a driver for the PCM2912A…
Part Number: PCM2912 Hi,
We are looking for an USB audio CODEC were we can chenge the audio decription shown in Windows (not PID/VID). It is nt possible with the PCM2912. Do you have other possibilities?
If not with CODEC, maybe with DAC and ADC combination…
Part Number: PCM2912 Tool/software: Linux Dear,
Our ctm want to use PCM2912; and the software environment is linux.
Could we can provide this device drive in linux system? Thanks!
Best regards
Part Number: PCM2912A Other Parts Discussed in Thread: PCM2912PCM2912_Audio.pdf
After running for a period of time, 3 out of 10 devices experienced an output of 0. Check that the power supply and input are normal. Attached is the schematic diagram. Could…
Hi MJ,
What setting you want to change in PCM2912, we have all of the software setting in USB descriptor, you can follow with the datasheet. volume control and mute control for input and output channel are already integrated into USB interface as below…
Part Number: PCM2912A Other Parts Discussed in Thread: PCM2912 , I have a trouble. When VBus and GND connect to power supply, XTIO will generate sin wave with 6 Mhz. But when PCM2912 connects against PC, XTIO out cannot keep generating the sin wave. But…