Part Number: PCM3002 Other Parts Discussed in Thread: TLV320AIC3204 , TLV320AIC3104
HI
i use PCM3002 to test audio
1: the test block is showed in the below
all power input pin is 3.3V
But Vref1 =3.3V
Vref2= 0V
is this correct?…
Part Number: PCM3002 Hi All,
Now i am prepare the PCM3002 for the Bluetooth eSCO function.
I want to know how can i reset the PCM3002 correctly(use /reset or sysclk ?)
thanks for your help.
Other Parts Discussed in Thread: PCM3002 , PCM3003 , PCM3008 Hello,
We are trying to interface audio codec PCM3002 on TS4900 from Technologic.
There seems to be some issue with program registers and format setup on either Audio codec or Processor…
Part Number: PCM3008 Other Parts Discussed in Thread: PCM3002 Tool/software: Hello team,
My customer is having noise problem on PCM3008.
Details on the thread below. https://e2e.ti.com/support/audio-group/audio-internal/f/audio---internal-forum/1342711…
Hi, George,
Thanks for the feedback. Depending on the complexity of your design, we have a couple options for you. If you need a simple device able to convert from analog to I²S and receive I²S data to stream analog output, probably a device like…
Couldn't find any 5416 specific examples dma-audio, but here is the link for C5517 chip support library cslv3.03:
http://www.ti.com/tool/sprc133
Please download the same, and refer the following mcbsp-dma-audio example in c55_csl_3.03\c55xx_csl\ccs_v5…
Other Parts Discussed in Thread: PCM3002 Hello!
Can I create a DSP/BIOS Configuration File for the dsk5416 in CCSv5 in order to run the project "tone"
which is an example which come with CCSV3.1 ?
If yes how can I do it ?
If NO how can I run this…