Other Parts Discussed in Thread: PCM3003 e2e,
We have a customer asking for the PC Application that is used with the DEM-PCM3003 evalutaion board. I checked the PCM3003 product page on TI.com and didn't find it. Couldn't find a product page for the…
Brandon,
we do specify the gain drift and BPZ drift over temperature for PCM3003 and uwe do not have char data for the output drift at 3.3V for the same.
Best regards,
Ravi
Hi, Lawoo,
Welcome to E2E, Thanks for your interest in our products!.
The PCM3002 is a quite old device which has limited support options, unfortunately we don't have a device which can be used as a direct replacement. The PCM3003 has the same package…
Hi, Prashant,
From the information you shared, it seems the issue is related to a clock error, this device expects to have 32, 48, or 64 bit clocks in one word clock, otherwise the clocks will be considered as invalid. In your application, BCLK has…
Sarmad,
The AUDIO16 card's link mentions the C6713 DSK several times and claims to have example software for that board. That certainly tells me that the boards are compatible.
Interrupts are not the same as data channels, so your question does not…
HI
i see the attached document
20bit data
CPLD input clk=12.288 sampling rate fs=8khz
codec sysCLK=2.048MHz
LRCIN=fs=8khz
BCLKin=CODE_SYSCLK/4=512K ?
How to get 4?
example.pdf