Hi Jeff,
using PCM3070rhbevm rev a. on top of USB-MODEVM board. This is recognized by PurePath Sudio Home Audio GDE as :
MWIDTLV320AIC32-4EVM-K; The GDE locks up with only the Framework PCM30702x 1x.
I then downloaded :
TLV320AIC3204EVM-K -SLOC128
…
Other Parts Discussed in Thread: PCM3070RHBEVM-K , PCM3070 TI,
I just got the PCM3070RHBEVM-K and PurePath...
I tried to download and run the Example (PCM3070_Example1_PFW) and I get the following:
Output Window Found board type: ????????????????????? …
Other Parts Discussed in Thread: PCM3070 , PCM3070RHBEVM-K Good day
I have PCM3070RHBEVM-K and USB-MODEVM interface board worked well with connection to PC.
If I want use PCM3070RHBEVM-K board only and connect to other MCU host (no connection to PC),
what is…
Other Parts Discussed in Thread: PCM3070 , PCM3070RHBEVM-K I just received my PCM3070RHBEVM-K and USB_MODEVM Interface boards yesterday. I followed the PCM3070EVM-K Evaluation Module User's Guide (slau331a.pdf) to verify the switch and jumper configurations…
Newer EVMs (~2007+)
The EVM User Guides for the devices below have been updated to include instructions on how to use these EVMs under Windows 7. Click a device, open the User Guide and search "Windows 7".
For the devices below, the EVM firmware…
To start miniDSP code development, you need to:
1. Obtain an EVM:
TLV320ADC3101EVM-K TLV320AIC3111EVM-K TLV320AIC3120EVM-U TLV320AIC3253EVM-K TLV320AIC3254EVM-K TLV320AIC3254EVM-U TLV320AIC3256EVM-U TLV320AIC3262EVM-U TLV320AIC3263EVM-U TLV320AIC3268EVM…
Hi Luis
There is no problem with Pure Path Studio, I have PurePath Studio(Home Audio) ver 5.95.
I mean current firmware of PCM3070RHBEVM-K (V3.54) maximum support only 48kHz.
Do you have firmware of PCM3070RHBEVM-K which suppot rate 88.2kHz and 176…
Part Number: PCM3070 Hi, I use PCM3070RHBEVM-K DEMO and download the software.Now,
I use the PCM3070 to make 2.1 speakers and line out as the Treble output , and the headphone as the Bass output
But I don't know how to set high and low bass cutoff…
Other Parts Discussed in Thread: PCM3070RHBEVM-K , PCM3070 I have a problem in first steps with PCM3070RHBEVM-K and PurePath Studio. There is an example named PCM3070 Example 1 PFW.
Input over Line IN1 J1 and output J7 Line out.
There is nothing. I changed…