Part Number: PCM3120-Q1 Other Parts Discussed in Thread: PCM3140-Q1 , Tool/software: Hi team
PCM3120-Q1 and PCM3140-Q1 are designed in my customer DHU board. Customer wanted to get the reference code in Luux. Would you help provide them?
Thanks
Part Number: PCM3120-Q1 Other Parts Discussed in Thread: PCM3140-Q1 , Tool/software: Hi BU team
Customer checked the datasheets of pcm3120-Q1 and pcm3140-Q1 and found the power-up and power-down sequence are different.
Would you help share your comments…
Part Number: PCM3120-Q1 Hi Team
My customer ZID wanted to know what's meaning on PCM3120-Q1 ASI input mixing saturation alter. Can not find any description on this interrupt in the datasheet. Thanks
Part Number: PCM3120-Q1 Hi experts,
Can we leave GPIO1 open when it is not used?
If No.1 is yes, do we need to disable the GPIO through GPIO_CFG0 register? or default IRQ setting is OK?
If No.1 is no, what is the recommended termination and GPIO1…
Part Number: PCM3120-Q1
Tool/software:
Hello everybody,
I have a problem with the PCM3120-Q1, where I measue data with the I2S interface.
I apply a sine wave with 5 kHz on the input of the ADC.
When I configure the I2S interface with 96 kHz…
Part Number: PCM3120-Q1 Hi team,
In datasheet 8.5.1.1, I understood 2x PCM3120-Q1 can be connected at the same time. Is my understanding correct?
Regards,
Youhei MIYAOKA
Part Number: PCM3140-Q1 Other Parts Discussed in Thread: PCM3120-Q1 ,
Hi team
My customer wanted to confirm if it is supported that fsync and data is transmitted on the falling edge of BCLK when PCM3140-Q1 and PCM3120-Q1 work under TDM slave mode…
Hi Garret-san, I'd like to make sure about your previous suggestion. You suggest us to use PCM3120-Q1 if customer need 24bit data. However, at that time, you may had wrong understanding for customer requirement as we talked.
Then, Can PCM3120-Q1 output…