Texas Instruments wide portfolio of Audio features Audio Converters , Audio Amplifiers and other Audio interface devices that are potential crosses for Discontinued, NRND or EOL Cirrus Logic Devices listed by Cirrus Logic here .
TI potential crosses in the…
The PCM3168A and the PCM3168A-Q1 are commercial and automotive, multi-channel CODECs that are a great replacement option for AK4628. The PCM3168A is the only multi-channel CODEC available with a 6-channel, 107dB SNR ADC and an 8-channel, 112dB SNR DAC…
Part Number: PCM3168A Other Parts Discussed in Thread: TLV320AIC3109-Q1 Hi,
I am planning to use PCM3168APAP for my Mono Audio In and output interface. Can you confirm whether the IC supports Mono or stereo audio interface.
Hi Jian,
Could you please help me with following -
1) Where and how should I enable MCASP0 (or k3-j721e-common-proc-board-infotainment.dtso) in uboot environment?
2) In k3-j721e-common-proc-board-infotainment.dtso overlay It is pointing to "pcm3168a", whereas…
Part Number: PCM1862-Q1 Other Parts Discussed in Thread: PCM1862 , , PCM1860-Q1 , PCM1840 , PCM3168A Hi
Since customer needs TDM, and two or four simple channels audio ADC, no gain control is needed. Does PCM1862-Q1 work without I2C Configuration? Or say can…
Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: PCM3168A hi, when testing the tienc_encode with some yuv videos,
with cmd: ./tienc_encode -i akiyo_cif.yuv -w 352 -h 288 -b 1000000 -o image.h264
I met a WARNING:
query_ctrls name=H264 I period…
Part Number: PCM6260-Q1 Other Parts Discussed in Thread: PCM3168A , TLV320AIC3268 , SRC4194 Hi team,
I am looking for replacement for competitor AKM devices as below, could you help to share some advice? Doesn't have to pin to pin, could be functional compatiable…
Part Number: AM5728 Other Parts Discussed in Thread: BEAGLEBOARD-X15 , TLV320AIC3104 , TLV320AIC3204 , PCM3168A-Q1
Hello,
I need to output 8 audio channels (each receiver would be single channel; 2 wire; 600Ohm) from a AM5728.
I read on the documentation…
Other Parts Discussed in Thread: PCM3168A-Q1 , PCM3168 , PLL1707 Hi:
Im designing a multichannel audio cape for BeagleBoneBlack, using the PCM3168A-Q1...
I wanted to ask if i should connect SCKI of the codec to an externall codec or if there is a pin of…
Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: PCM3168A Hello Sir
I am trying debug the usb net driver. But it seems that the usb device can not be identified.
when I using lsusb, there is no any info output. Below is the full log, could you please…