Part Number: PCM4201 Other Parts Discussed in Thread: OPA1632 I am considering a circuit that uses an OPA1632 differential amplifier in the front stage of the PCM4201. I need to connect a reference voltage to the VOCM pin of OPA1632, but is it okay to…
Part Number: PCM4201 Other Parts Discussed in Thread: ADS1271 , , THS4551 Hi,
I was using ADS1271 which offers a good DC and AC performance.
At the moment, the part is out of stock, so I'm considering replacing it with a PCM4201.
My application needs…
Part Number: PCM4201 PM4201
What's the difference between master mode and slave mode of PCM4201; what applications are they used for, in my case, I want to realize sound source localization via microphone arrays, and I will use FPGA as controller.(By…
Part Number: PCM4201
Hi,
I have a higher than expected failure rate for the PCM4201. On 3 chips the audio performance was below the correct quality standard. It was found that the voltage across the Vref pins was wrong (e.g 4.2V), instead of the 2.5V…
Part Number: PCM4201 Hi E2E, Good day. The datasheet shows the frequency response of the device start at 20Hz. Can you provide any frequency response plots for 20Hz to 1Hz? Our customer will be using the PCM4201 to measure the output of an amplifier that…
Part Number: PCM4201 Dear TI
I'm debugging PCM4201 because audio noise.
1. System block
2. Mode setting(Master or Slave)
- We are using 11.025KHz sampling frequency.
- Which mode(Master or slave) can be set?
> Slave: 256fs or 512fs
> Master: …
Part Number: PCM4201 Other Parts Discussed in Thread: PCM5102A , , PCM4202 Hi Team
We design a audio system use PCM4201+DSP+PCM5102A, but we can't get the right date from PCM5102A. We have some question need to confirm. thank you
1. Can PCM4201 support…
Part Number: PCM4201 Dear TI
I'm Hardware Engineer at Intek Digital in South Korea.
I'm under implementing using your PCM4201 Audio ADC.
I have two question about PCM4201.
This is very urgent issue, please help me ASAP.
1.
1)According to datasheet…
Part Number: PCM4201 DEARS.
The PCM4201 input type is difference.
Can I PCM4201 analog input type be used as Single-End?
What is the SE input type product with a similar specification of pcm4201?
Thank you.