Part Number: PCM4201 DEARS.
The PCM4201 input type is difference.
Can I PCM4201 analog input type be used as Single-End?
What is the SE input type product with a similar specification of pcm4201?
Thank you.
Part Number: PCM4201 Hello, I'd like to ask about audio ADC, PCM4201.
Is there any plans for discontinuance PCM4201? It seems old product.
Best Regards, Kazuto Tatsumi
Part Number: PCM4201 Other Parts Discussed in Thread: PCM1804 , Hi,
The PCM4201 and PCM1804 both offer the ability to bypass the internal high pass filter. I know these are not designed for DC applications and are not specified for DC error.
But would either…
Part Number: PCM1821EVM Other Parts Discussed in Thread: PCM1821 , PCM4201 , DRV134 Hi
PCM1821 transmits 32-bit two-channel data. The customer's product actually only has a mono signal. When the back-end MCU receives the I2S dual-channel data, it needs to…
Hi Colin,
Sorry to hear that. Please feel free to come back with any additional questions you have, if you have time to take another look there is an EVM Users Guide you can compare your setup/PCB schematic to: www.ti.com/.../sbau108a.pdf
Justin
Other Parts Discussed in Thread: ADS1271 , PCM4201 I am looking for specification of antialias filter applied in PCM4201 ADC. I have recognized A-A filter in ADS1271 - is the characteristics same or similar?
Regards
Artur
Other Parts Discussed in Thread: DIX4192EVM-PDK , PCM1748 , PCM4201 , DIX4192 Hi everyone! We are currently planning to evaluate our design of an audio related project. We are using ADC (PCM4201) and DAC (PCM1748) on our board and we would like to test them…
Other Parts Discussed in Thread: PCM4201 , PCM1774 Hi All, Would you mind if we ask PCM4201 and PCM1774? <Question> These PCM4201 and PCM1774 are used for audio(AC) generally. However, if we use as DC signal(0Hz), are these devices available to use DC signal…
Other Parts Discussed in Thread: PCM4201 The PCM4201 datasheet says that the ADC reference voltage is "an on-chip band gap reference for the delta-sigma modulator, eliminating the need for external reference circuitry"
Is there any information…