Part Number: PCM4204 I am trying to understand how the Oversampling Ratio of this ADC is defined. Would I be correct in assuming the OSR rates are listed in Table 1 as 128fs, 192fs, 256fs, 384fs, 512fs and 768fs ? If true, why does Sampling Modes paragraph…
Part Number: PCM4204 Hi team,
Let me ask questions about power requirements.
1. Is there any requirements of power-on/power-off sequence of Vcc and Vdd? If I understand correctly, RESET OPERATION section describes initialization sequence, but this…
Part Number: PCM4204 We observe that the THD vs. frequency performance varies between channels while SNR stays the same. Is this expected, and if so, what influences the variations in THD performance?
Part Number: PCM4204 Other Parts Discussed in Thread: PCM4202 Hi team,
I know that it shows PCM4202 can operate during -10℃~70℃(datasheet maybe conservative ). But customer's work condition will be up to -45 °C – 85 °C, so whether PCM4202 can afford…
Hello Ravi:
you mean that the short-frame data structure in Fig4 of PCM4204 DS is wring?
two more questions:
1. IF want use PCM4204 in slave mode,and we want set the Fs equal to 96KHz,then how to set the SCKI and BCK frequency?
2. we want to get…
Part Number: PCM4204 Hello,
I've been noticing a fair amount of low frequency noise coming from this chip, which is in the A/D section of a presonus audio interface I recently overhauled. In the image below, there's that spike that looks to be near…
Part Number: PCM4202 Other Parts Discussed in Thread: PCM4204 Hi,
In order to input a single-ended signal to PCM4204 with minimum space/component requirements, despite high performance, is it possible to use a single OpAmp as specified in this design…
Part Number: PCM4204 Hi team,
I have a question coming from a customer.
For the PCM4204, do the analog inputs (VIN1, VIN2, VIN3, and VIN4) correspond or relate to the LRCK in I2S mode in anyway? If so, how?