Part Number: PCM5100 Hi
How to operate: CPU's I2S -> DAC Analyst -> AMP (TPA3118D2DAPR) -> Internal Speaker Output
Audio output port: HDMI for setting and controlling audio output via TV and built-in speakers
Symptom : During AC POWER OFF…
Part Number: PCM5100 Hi team,
My customer asked for Input overload level of PCM5100.
But I haven't heard of this parameter. Would you let me know?
Thanks
Jay
Part Number: PCM5101A Other Parts Discussed in Thread: PCM5100 , PCM5101 Dear TI Team
Please tell me the difference between PCM5101A and PCM5100. When I check the data sheet, it seems that there is a difference in the power supply voltage value. If there…
Part Number: PCM5100
Hello,
The suggested LPF on the PCM5100 DAC output is 470E and 2.2nF that gives a cut-off frequency of around 154KHz.
For the purpose of minimizing the unique parts in my BOM, I would like to use 316E and 3.3nF that would have a…
PCM5100 or any DAC you pick, converts digital signal to analog signal and reconstructs the input amplitude and frequency ( within a margin of error that datasheet may have mentioned) . As far as I know, in PCM5100 we have no control to adjust the reconstructed…
Part Number: PCM5100 Other Parts Discussed in Thread: , DAC8871 , PCM1794A , DAC80501 , PCM5122 , PCM1690 Hello,
Please advise if multiple PCM5100s can be made to work in phase i.e., the outputs are phase synchronous. Also, will there be any delay between…
Part Number: PCM5102EVM-U Other Parts Discussed in Thread: PCM5121 , PCM5100 Hi
We are now evaluate PCM5102EVM-U, our setup as below
1. remove all jumper from W3
2. I2S signal feed to W3 pin 20, 22, 24, and 26 with
SCK = 5.6MHz
BCK = 2.8MHz
LR clock…
Part Number: PCM5100 Hi team,
We used PCM5100EVM-U for experiments. The I2S audio signals BCK, LRCK and DIN are inputted to the PCM5100, and the BCK, LRCK, DIN pin waveforms are right, however, there are no outputs.
The switches are configured as following…
Part Number: PCM5100 Other Parts Discussed in Thread: PCM5101 Hi
I got one PCM510xEVM-U and I'd like to convert USB audio streaming to analog output,
After booting up with "PCM5101_Init.txt" and then I load and run "PCM5101_USB Playback.txt",…
Part Number: PCM5100 Other Parts Discussed in Thread: PCM5102EVM-U Hi team,
My customer is using PCM5100 in car audio. Recently they have test EMC noise in Pin 2/4, as show below, could I have you comments why they can see such EMC on Pin 2/4?
I upload…