Part Number: PCM5101 In the asm3m project, Ti pcm5101 produced 200 sets, and 4 sets were shut down with obvious pop sound. It can be measured that the 6 and 7 pins of pcm5101 have waveform output.
Can you help me check the problem.
The schematic diagram…
Part Number: PCM5122 Other Parts Discussed in Thread: , PCM5101 We are trying to run the PCM5122 with a sample frequency of 256kHz and a SCK/BCK of 16.384MHz.
We are running in SPI mode and see no output despite configuring all of the registers correctly…
Part Number: PCM5101 Hi team.
My customer requested schematic review.
Schematic of customer is confidential.
Please let me know contact email.
I will share the schematic to the associated engineer.
Thank you.
Other Parts Discussed in Thread: PCM1754 , PCM1789 , PCM5101 , PCM5102 , PCM5100A , PCM5100 Hi, TI support team
Please recommend a product that meets the conditions below.
- Overall performance: same or similar product as PCM1754
- I2S (SCK, LRCK, BCK, Dats…
Part Number: PCM5101A Other Parts Discussed in Thread: PCM5102A Dear Support team,
My customer will use PCM5101A in their AVR application.
They are in trouble with the peak noise appearing at 48 kHz and 96 kHz.
AVDD = CPVDD = DVDD = 3.3 V, fs = 48 kHz…
Marvin,
would you please ask them to do a register dump to make sure the address of the device they are using is what it is supposed to be ( For example if the address is 98 but they are using E0, it can not communicate with the IC).
I checked the register…
Part Number: PCM5142EVM-U Other Parts Discussed in Thread: PCM5101 , PCM5142 Hi Team,
Can you please check the inquiry below?
Using PCM5142EVM-U, if you look at this schematic below, there is a signal called: WCLK and I read on the datasheet TAS1020B has…
Part Number: PCM5142EVM-U Other Parts Discussed in Thread: PCM5101 , PCM5142 Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
A recent inquiry from the customer was posted in the link below. e2e.ti.com/.../pcm5142evm-u-registers-…